Part Number: SN74AXC8T245-Q1 Hi team,
I have one question about SN74AXC8T245-Q1. We plan to use this device for 1V8 to 1V8, the purpose is to pull high /OE pin to disconnect the RGMII(125Mhz) signal before the whole system bring up.
My question:
1. Can…
Hi David,
Thanks for reaching out. It would seem your concern seems to be a duplicate of SN74AXC8T245-Q1: SN74AXC8T245-Q1 .
If so, could you please help confirm if working with Barton Tung's team as we have further clarified offline with additional solutions…
Part Number: SN74AXC8T245-Q1 e2e,
I had an understanding that VCCB_1(pin23) and VCCB_2(pin24) were tied separately, so that VCCB_1 powers bit 1 to 4 and VCCB_2 powers bit 5-8. However, from the datasheet it seems like VCCB pin 23 and pin 24 is common…
Part Number: SN74AXC8T245 Other Parts Discussed in Thread: SN74AVC8T245 , DP83TG720R-Q1 , TXV0106-Q1
Hi,
I am using DP83TG720R-Q1 1000BASE-T1 Automotive Ethernet PHY. This will be connected to ZU-7 SoC from AMD. The I/O voltage supported by SoC is 1.2V.…
Part Number: SN74AXC8T245-Q1 Hi
There is no skew parameter in SN74AXC8T245-Q1 datasheet, and TI engineers has ever said that typical channel-to-channel skew is 150ps-200ps for 1.8V← →3.3V case, my question is that:
1. whether I can use 150ps…
Part Number: SN74AXC8T245 Other Parts Discussed in Thread: DAC900 , , TXV0108-Q1 , TXV0106-Q1 Hi team,
When I use multiple SN74AXC8T245s , what is the skew between the devices?
The system has 11 bits of clock and data, so I am concerning.
(I understood from…
Part Number: SN74AXC8T245-Q1 Hello,
Is the Pad of the CAXC8T245QRHLRQ1 internally connected to ground? The datasheet does not appear to specifically specify one way or the other. It says it can be left floating or connected to ground, but does not indicate…
Part Number: SN74AXC8T245-Q1 Other Parts Discussed in Thread: SN74AXC8T245 Hi, Clemens
I have two questions about SN74AXC8T245-Q1.
1. In datasheet, I didn't find the channel-to-channel skew specification, so what's the skew value?
2. In document…
Part Number: SN74AXC8T245-Q1 Hello,
I'm looking at the SN74AXC8T245-Q1, however the datasheet doesn't seem to indicate rise time for the output drivers for this part. I see the enable and disable times, but could TI advise the minimum Rise and…