Part Number: SN74CB3Q3125 Hi team,
We have some questions about the SN74CB3Q3125PWR.
1. whether the input is the mosfet structure?
2. whether the input can accept higher negative voltage -2v with smaller time(20ns)?
3. What's the meaning of VIK?-1.8V.
Thanks…
Part Number: SN74CB3Q3125SN74CB3Q3125 datasheet specified support with USB interface application, Can SN74CB3Q3125 also support with CAN BUS application which BUS switch in between Microprocessor and Transceiver? Thanks.
Part Number: SN74CB3Q3125 Other Parts Discussed in Thread: SN74CB3T3125 , E2E,
Would sn74cb3t3125 be a higher current allowance to sn74cb3q3125 ? What is the difference between the two?
Thank you,
Adam
Shinu,
Please see this post I found by typing "SN74CB3Q3125 drive strength" into the switches and multiplexers search bar.
Please let me know if the above post answers your question.
Thank you,
Adam
Part Number: SN74CB3Q3125 Other Parts Discussed in Thread: TS3A4751 , Hi Sirs, My customer is evaluating a SPST switch SN74CB3Q3125 and asking us to provide more information on its isolation characteristics. What my customer need is very similar to below diagram…
Part Number: SN74CB3Q3125 Hi Team,
I have a quick question our customer would like to clarify, can the SN74CB3Q3125 device be used to interface with an open drain driver/receiver circuit? Or does it only work with LVCMOS/LVTTL IO buffers?
Thanks and…
Bhargav Goud,
The SN74CB3Q3125 is a bidirectional passive FET switch and does not have any drive capability. You will need to check the driver that is external to the switch if it can provide the required drive strength.
The SN74CB3Q3125 datasheet states…
Part Number: SN74CB3Q3125 Hi,
I am trying to understand why I see some a short voltage spike at the output of the SN74CB3Q3125 in the switch off state.
Red Trace: Input to Switch
Gold Trace: Enable Signal
Green Trace: Output Signal from Switch (Zoomed…
Part Number: SN74CB3Q3125 Hi all,
Simple question: is the center pad connected to ground within the part? 99.9999% of the time it is. However, I don't see a specific call out for the pad connectivity in the Datasheet. So I'm asking to be better safe than…
Part Number: TMUX1511 Other Parts Discussed in Thread: SN74CB3Q3125 Hi,
I would like to know what is the maximum propagation delay of TMUX1511? Similar devices such as SN74CB3Q3125 are specified in the datasheet as the maximum propagation delay 0.2ns@3…