Part Number: SN74CB3Q3345 Other Parts Discussed in Thread: TXB0108 , TXB0102 , TXS0102 Hello TI Team, I would like to inquire about the feasibility of the following concept or seek expert advice on suitable TI product models. We have a new project that involves…
Part Number: SN74CB3T3245 Hi
My customer wishes to know the key differentiation on abovementioned devices.
I checked through ti.com device comparison tool, it shows the BW is different but i couldn't see those parameter recorded the datasheet,
Could…
Part Number: SN74CB3Q3345 Other Parts Discussed in Thread: SN74CB3T3245 , SN74CB3Q3245 Dear Specialists,
My customer is considering SN74CB3345 instead of SN74CB3245.
They have a question about OE pin.
I would be grateful if you could advise.
---questi…
Part Number: SN74CB3Q3345 Other Parts Discussed in Thread: TS3A27518E , SN74CBT3125 team,
In notebook application we noticed that for SPI bus switch Intel spec the Cin as <3pF. sn74cb3q3345 has a typical of 2.5pF while 3pF as the maximum.
Will it be…
Part Number: SN74CB3Q3345 Team,
is it ok (or even needed) to connect the thermal pad to GND?
My customer cannot find that information in the datasheet.
Thanks!
Part Number: SN74CB3Q3345 On page 1 of the datasheet, the pin out diagram for the RGY package shows pin 16 is "B9", and there is no "B3". Is pin 16 supposed to be "B9"?
http://www.ti.com/lit/ds/symlink/sn74cb3q3345.pdf
Thanks…
Part Number: SN74CB3Q3345 HI,
SN74CB3Q3345 datasheet contains content below: "Rail-to-Rail Switching on Data I/O Ports".
Does it mean, the output Voltage Level is the same as the input, regadless of the Vcc supply?
For example, the Vcc supply…
Other Parts Discussed in Thread: SN74CB3Q3345 Question regarding SN74CB3Q3345 in partial power down:
When Vcc, OE, and OE/ are 0V, is there isolation between the A and B lines?
The notes about partial power-down are vague and I can't determine if there…