Hi Malik,
ADS8688 doesn't have a command to disable the software reset command(8500h). There are two solutions which could be used:
1. Make your circuit and system robust by improving pcb layout or other ways on system level, No interference signal…
Martin,
I would also like to point out you can search for this IOFF or powered off isolation feature on our TI.com switch selection tool . I filtered the tool for 1 and 2 channel, 1:1 SPST devices with the IOFF feature you are looking for.
…
Most of our Cmos buffers will translate down to Vcc
SN74AUP1G125 for low power consumption
SN74CB3T1G125 For almost no delay
We have some duel voltage translators SN74LVC1T45 or SN74AVC1T45 for a single bit.
These all come in many bit widths…
Hi Bill Albrant,
the MSP430FR5739 can run at up to 24MHz! Yes, it is a 3.6V (max) device, but where's the problem? When you need to connect it to 5V peripherals you can use level shifters i.e. like the TXS0104E (4-bit OD) or SN74CB3T1G125 (1-bit);…