Part Number: SN74CBT16209A Other Parts Discussed in Thread: SN74CBT16212C Hi Expert,
Because I can't find the simulation model on TI website, could you help to share it with me?
Regards,
Mark
Part Number: SN74CBT16209A Hello,
I would like to use the SN74CBT16209AD as a two 9-bit bus multiplexer, only using the functions A1=B1 or A1=B2. I will supply the chip with 5VDC and I do not want to perform any level translation. I would like to clarify…
Part Number: SN74CBT16209A Other Parts Discussed in Thread: TMUX1574 , TS3A27518E
Studying SN74CBT16209A for a SPI application
can SN74CBT16209A support SPI Quad IO application with bi-directional ?
can ISN74CBT16209A support SPI Clock run with…
Part Number: SN74CBT16209A Hello,
I am designing a circuit with the SN74CBT16209A with the following configuration:
Input signals: 3.3V TTL
Control signals: 3.3V TTL
Vcc=4.3V
I would need some help with the following questions:
- Is the Vg…
Part Number: SN74CBT16209A Other Parts Discussed in Thread: ADS8688 , SN74CBT16232 Hello All,
I have an application to read two 16 bit Bus (ADS8688 data). But I don't have sufficient GPIO pins to read the Bus.
So, I am looking for a multiplexer to…