Part Number: SN74CBT3244 Other Parts Discussed in Thread: , TXB0304 , TXU0104
Hi We are using a circuit like shown in the below image.
A programming header is provided for programming the device for the first time. A header logic is implemented for OE#…
Part Number: SN74CBT3244 Other Parts Discussed in Thread: SN74CBTLV3245A , SN74CB3Q3244 Hi Experts:
Customer use SN74CBT3244 as switch in PDB, enable signal is FM_SLED_PWRGD and circuit as below.
And they found the SMB_PSU_PMBUS_ALRT_N (pin5) of U2 only…
Part Number: SN74CBT3244 Other Parts Discussed in Thread: SN74CBT3245A Can SN74CBT3244 be used as a de-multiplexer? This is not explicitly stated in the Datasheet, but comparing against SN74CBT3245A (which does say it is bidirectional) they seem to be…
Part Number: SN74CBT3244 Hi Team, Can SN74CBT3244 be used for level shifter for open drain application by adding pull-up resistors? I assume 5V to 3.3V purpose. Best Regards, Yaita / Japan disty
Other Parts Discussed in Thread: SN74CBT3244 , SN74LV4066A , SN74CBT3345 , CD4066B Hi team,
Do we have a Multiplexer device which can support 8 input/8 output and every Chanel can be enable or disable?
Thinks!
Part Number: DRV8303 Other Parts Discussed in Thread: DRV8308 , SN74CBT3244 HELLO the problem is my DRV burned after a fews minutes. The VM pin have 9 V (the minimum in data sheet is 8.5V ) this is because i need to communicate with them over SPI to read…