Part Number: SN74CBT3251 Other Parts Discussed in Thread: TMUX1208 , TMUX1108 , Tool/software: Hi,
I'm currently using this part as demultiplexer to drive relays. Part is designed as picture shows:
VCC and COM pin are sharing same 5V bus which is driven…
Part Number: SN74CBT3251 Other Parts Discussed in Thread: SN74LV4051A , SN74CBT3253 , SN74CBTLV3251 , SN74CB3Q3251 , Hi team,
Due to shortage of SN74CBT3251RGYR, could you please help compare SN74CBT3251RGYR with SN74CBT3253, SN74LV4051A and SN74CBTLV3251?
…
Part Number: SN74CBT3251 Hi Experts;
I have questions on the SN74CBT3251, please the schematic below,
The B2 and B1 is input the voltage signal generated by the resistor divider, the output (A port) is connect to the input of the ADC (high impedance input…
Part Number: SN74CBT3251 Hi Team,
SN74CBT3251 was used in customer. The input PinB1~ B7 was shorted TO ground randomly when SN74CBT3251 was used to sample temperature.Here is the schematic for SN74CBT3251. The failure rate is 2%.
This is a special application…
Part Number: SN74CBT3251 Hi, Our customer checked RDSON under the following condition. ①Vcc=5V,A=5V,Rload=2Mohm or 470ohm ②Vcc=4.5V,A=4.5V Rload=2Mohm or 470ohm
At condition ①, the output voltage is 4.08V (Rload = 2Mohm) or 3.64V (Rload = 470ohm). Also, at…
Part Number: SN74CBT3251 Other Parts Discussed in Thread: MUX506 , SN74CBTLV3251 , SN74CB3Q3251 , TMUX1208 Dear sir,
There is a problem when I use multiplexer SN74CBT3251. The signal source is an 50 MHz optical receiver which convert the optical on/off to…
Part Number: SN74CBT3251 Other Parts Discussed in Thread: SN74CB3Q3251 , TMUX1208 , SN74CBTLV3251 Hi,
I have a question regarding SN74CBT3251D:
1.The datasheet doesn't seem to specify what the Vout max is(when using a 5V supply), nor what the Vout min is…
Part Number: SN74CBT3251 Other Parts Discussed in Thread: SN74CBT3253 , , TMUX1208 Dear Specialists,
My customer is considering SN74CBT3251 and SN74CBT3253.
He has a question, so I was wondering if you could advise.
---
Regarding SN74CBT3251 and SN74CBT3253…
Part Number: SN74CBT3251 Other Parts Discussed in Thread: SN74CB3Q3251 , Hi there:
We're looking for an solution with 1:8 Mux/De-Mux Bus switch, original solution: SN74CB3Q3251 couldn't support up to 25MHz.
Dose SN74CBT3251 could support switching…