Part Number: SN74CBTLV16212 Tool/software: Hi all,
I would like to use this component between a NOR flash and a FPGA.
About the I/O, are they directional: A1 to B1 , B1 to A1, A1 to B2, B2 to A1 ?
Is there any needed to have pullup resistors on the I…
Part Number: SN74CBTLV16212 What is the maximum frequency this switch can work with. Specifically we want to use this for the 100MHZ Flash interface switching over, is there any concern we should be care of? Thanks.
Part Number: SN74CBTLV16212 Other Parts Discussed in Thread: SN74LVC1G04 , PCF8575C I want to estimate the power consumption of my design. How can I do it for sn74cbtlv16212? At page 5, ICC is stated as 10uA, but ΔICC is a bit confusing.
Plz clarify…
Part Number: SN74CBTLV16212 Other Parts Discussed in Thread: SN74CBTLV3125 Hello,
Since its VCC supply voltage range is 2.3V~3.6V, I give a 3.3V supply on VCC,but signals on both port A and B are all 1.8V level such as LVCMOS-18 standard IOs.
Is that…
Hello Dhaval,
The SN74CBTLV16212 has two functionalities, you can use this device as a 12-bit bus cross point exchange switch or as a regular 24-bit switch.
Unfortunately, we do not offer the 12-bit exchange functionality at an automotive qual at this…
Part Number: SN74CBTLV16212 Hi,
Iam using IBIS model of SN74CBTLV16212 for simulation. I want to do simulation for A1 to B1 port.
Usually when using hyperlynx,
In the Pins list, when you select a pin connected to a series bus switch, all the other pins…
Other Parts Discussed in Thread: SN74CBTLV16212 , TS3A5017 I am not able to fine 1 to 4 channel 12 bit bus switch. I want to create a 1-4 channel bus switch by cascading 2 SN74CBTLV16212. Can i do this? I wanted to know the typical voltage drop across input…
Hi Krunal,
We have a D latch (sn74cbtlv16212) between AM3352 and NOR flash and ALE signal connected to D latch.
From NOR flash point of view it is not multiplexed. As far as processor is concerned it is multiplexed. We discussed this in below link.
https…
Hi Sanjay,
Besides SN74CB3Q16811, We have mutiple 24 bit bus cross switches such as SN74CB3T16212, SN74CBT16212C, SN74CBTLV16212, SN74CBT16212A, SN74CBT16213, SN74CBTS16212.
I would like to contact you to learn which part you think is better for Q1…