Part Number: SN74HC14 Hi All,
I have a question on SN74HC14.
Please tell me the value of VOL when VCC = 5V. I think it is difficult to answer, but please let me know if there are any reference values such as the VOL ability value when VCC = 5V.
Also, will…
Part Number: SN74HC14 Hi Team, In reference to the original post, does the recent change to the die size affect or change the fit of the device on a board with the older version installed? Kind Regards, Jejomar
Part Number: SN74HC14 Other Parts Discussed in Thread: UCC27517 , SN74LVC1G14 Hi Team
When using Schmitt triggers to control MOS , but the output current does not reach the current required for MOS conduct (e.g. Schmitt triggers single channel maximum output…
Weijie Gao said: If the problem still cannot be solved, can you send it back to the original factory for testing? It is suspected that there is a quality problem in this batch.
You can start an FA with your supplier -- I cannot help with returns here,…
Part Number: SN74HC14 Other Parts Discussed in Thread: CD40106B , SN74AHC14 , Hi,
Good Day. I have a customer who has a query about logic device. Please see below for his query. Thank you very much.
I am looking for an inverter with a specific input feature…
Part Number: SN74HC14 1 if give a rc curcuit in the input of 74hc14,the output state is a certain high during power up?
2 if the input of 74hc14 is pull down,the output state is a certain high during power up?
the curcuit is in the following file curcuit…
Part Number: SN74HC14 From the detail data sheet, it show SN74HC14DR with "NIPDAU | SN" at the "Lead finish/ Ball material" column but SN74HC14DRG4 with "NIPDAU " at " Lead finish/ Ball material". Are both the same part…
Part Number: SN74HC14 Hi,
I am planning to drive LED using 74HC14 which will sink current around 10mA.
The datasheet of 74HC14 does have "continuous current" IO specified for +/-25mA while IOH & IOL is tested for +/-5.2mA in recommended…
Part Number: SN74HC14 Tool/software: TI C/C++ Compiler Model :SN74HC14D, brand: TI, used for non-gate oscillator and liquid level detection on the luminescent chemical immunoanalyzer produced by our company, but the detection was not accurate recently…