Part Number: SN74HC164 Other Parts Discussed in Thread: SN74LVC1G17 , SN74LVC1G14 Hi,
my customer's schematic is as below: U3 and U1 are two SN74HC164.
On good board, the waveform is shown below (upper picture). On bad board, the waveform is shown…
Part Number: SN74HC164 Other Parts Discussed in Thread: SN74LVC8T245 , CD74HCT164 , SN74AHCT595
Hi,
I am using SN74HC164NSR for my project. What is the minimum,quiescent and typical current consumption of SN74HC164NSR. The datasheet only provide the…
Part Number: SN74HC164 Hi.
I have a few questions with regards to SN74HC164 which I'm planning to replace an On-Semi part.
1. Looking at the datasheet, timing requirement Tt is missing from the timing diagram. What is the definition of Tt?
2. The…
Part Number: SN74HC164 Hi team
When the customer tests the maximum current of pin7, GND, it is found that the instantaneous current is 54.5MA, which exceeds the current of 50mA indicated in the specification. The waveform obtained from the test is as…
Part Number: SN74HC164 Hi Team :
Could you help to confirm , how to calculate power consumption on worst case of SN74HC164 ? current ? , thanks.
Regards / Mark
Part Number: SN74HC164 My customer has always used 74HC164PWRE4 but now is being replaced by 74HC164PWRG4. Was there a PCN issued for this changeover? If so, please advise.
Part Number: SN74HC164 Hi,
customer use SN74HC164 in LED display board, have a problem is that when the power up, the AB pin are low and CLK is low, the output is random. the CLR pin is force to high by external reisistor.
I check the datasheet, when…