Where does this reference come from? Did the reference circuit not have C17/C18?
Anyway, I've already told you how to fix this: make the edges faster, or use the HCS device.
Part Number: SN74HC165
“We had heated and cooled the assembled electronics in the range of 35 and 60 degrees Celsius. The temperature change produced a curious error pattern: the serial output caused certain bits to flicker.”
Part Number: SN74HC165 Other Parts Discussed in Thread: SN74HCS165 , SN74LV165A , CD74HC165 , SN74HCS165-Q1 Is there p2p compatible one with new process as the Lead time of old one is not good? Pls recommend . Thanks
Part Number: SN74HC165 Other Parts Discussed in Thread: SN74HC595 , CD74HC299 , SN74LVC1G04 , SN74AHC1G04 Dear support team,
I am currently working at an GPIO extension for a microcontroller. I want to use 1 SPI Port for the extension with digital inputs…
Part Number: SN74HC165 Dear,
the datasheet Note 2: When Vcc = 2V, Tt =1000nS =1000nS /V x (1.5V-0.5V) ? If Vcc=4.5V, Tt= 500nS/V x (3.15-1.35)=900ns, the chip will not be damaged. As long as it is below 1.35V or above 3.15V, it is safe?
If not, please…
Part Number: SN74HC165 Other Parts Discussed in Thread: CD74HC165 , , SN74HCS165 , ISO7740 Dear,
the datasheet Note 2: When Vcc = 2V, Tt =1000nS =1000nS /V x (1.5V-0.5V) ? If Vcc=4.5V, Tt= 500nS/V x (3.15-1.35)=900ns, the chip will not be damaged. As long…
Part Number: SN74HC165 Other Parts Discussed in Thread: SN74AHC595 , Hi
I have a question to ask about the design of serial-to-parallel conversion design, which parts should be paid attention to, such as how to consider the bandwidth
Part Number: SN74HC165 Other Parts Discussed in Thread: SN74HCT165 , SN74HCS165 Hi team,
Hope you're well!
My customer recently swapped out a SN74 LS 165AD for a SN74 HC 165DR on their board and are now experiencing failures where they weren't before. Swapping…