Part Number: SN74HCS125
Hello team,
I am shweta chendake From knorr -bremse technology center india
in datasheet of SN74HCS125 the Input Vinh and Vinl values are missing could you please help with provideing these missing values?
also the rise…
Part Number: SN74HCS125-Q1 Tool/software: Hi team,
Can I use this device to buffer SPI signal(7.5MHz) in the system? I worry that there is some limit on this device.
Regards,
Peter
Part Number: SN74HCS125 Tool/software: i try to simulate pspice model of SN74HCS125PWR, but output is always zero without getting any error. can you please check that model is working or not.
Part Number: SN74HCS125 Other Parts Discussed in Thread: SN74AHCT125 , SN74LV4T125 Tool/software: Hi team.
If Vcc is 5V. when Vin is 3.3V. what is Vo value? thanks
Part Number: SN74HCS125 Other Parts Discussed in Thread: SN74LV125A , SN74LV14A , , SN74HCS14 , SN74AHC125 , SN74AHC14 Tool/software: Dear Technical Support Team,
Q1 Regarding SN74LV series, SN74HCS series and SN74AHC series Is it possible to provide…
Part Number: SN74HCS125-Q1 Other Parts Discussed in Thread: SN54AHC244-SP Tool/software: Hello experts,
We want to use SN74HCS125-Q1 to the satellite project.
Are there any restrictions on using it on satellites?
Best regards,
Toru Kimura.
Part Number: SN74HCS125 Other Parts Discussed in Thread: SN74LVC3G17 , SN74LVC2G17 Tool/software: Hi,
I am planning to use this buffer for SPI signals over cable.
Currently, on PCB all SPI signals are length matched in 300 mils with SPI CLK.
Now…
Part Number: SN74HCS125 Hi,
TI has so many logic IC with low-enable function(like 125,240,244,245).
Is there any specific reason that is still using low-enable ?
what is the advantage of Low-enable?
Thanks,
Go
Part Number: SN74HCS125 Other Parts Discussed in Thread: ESDS314 , SN74HC125 Hello Community,
We have a application where we want to interface the output of SN74HCS125 operating at 5V VCC to the MCU digital input pins which are 5V tolerant. The signal…