Part Number: SN74HCS86 Other Parts Discussed in Thread: SN74LVC86A ,
Hi Team,
Compared with sn74hcs86 and sn74lvc86A datasheet, I saw IIK support +/-20 mA (when VI < –0.5 V or VI > VCC + 0.5 V) in sn74hcs86 datasheet.
But sn74lvc86A just support…
Part Number: SN74HCS86 Hi Sir,
A customer need WQFN (BQA) 14pin package drawing, but I can not find it in the website and the datasheet.
It looks like a new package.
SN74HCS86BQAR
Can you share this drawing? dimension drawing and recommended footprint…
Part Number: SN74HCS86 Other Parts Discussed in Thread: SN74LVC1G58 Hi,
I am looking into designing a frequency doubling circuit using the SN74HCS86 (XOR) and a comparator. The input freq is ~50 MHz, so the doubled output is ~100 MHz.
Do you know what…
Part Number: SN74HCS86 Hello guys,
One of my customers is considering using SN74HCS86 for their new products.
They have a question about this device as the follow. Could you please give me your reply?
Q. Do you have Vt+ Positive switching threshold, Vt…
Part Number: SN74HCS86 Other Parts Discussed in Thread: TCA6424 , SN74HCS74 , Hi team,
My customer is testing SN74HCS86PWR. Customer selects this device because it has very low Iq. Customer found in room-temperature and high-temperature test, the Iq is normal…
About 8× is OK for digital signals.
The termination resistor should match the characteristic impedance of the cable. CAT6 usually has 100 Ω.
A differential transmitter outputs two signals that are inverted from each other. This can be done…
Hi Boyan,
If the requirement is just for an XOR gate, then I might recommend the SN74HCS86-Q1 available in the BQA package. Do we know any timing limitations or output loading concerns?
Pin 3 of the 555 outputs a regular square wave; you can indeed trigger on any edge. You can also replace the 555 with another source (which would be necessary for more than 2 MHz).
The top transceiver is used only as a transmitter; the bottom transceiver…
How have you connected the inputs of the fourth gate? They must never float.
What is the current through D2? Is the voltage at pin 1 ever between V IL and V IH ?
C2 makes the signal edges quite slow. You should use a device with Schmitt-trigger inputs like…
Part Number: SN74HCS00 Other Parts Discussed in Thread: SN74HCS86 ,
I see that there is a SPICE behavioral model for the SN74HCS86. This has been very useful in TINA/P-SPICE simulation.
Would it be possible to get a similar model for the SN74HCS00 NAND…