Other Parts Discussed in Thread: SN74LV08A , SN74AHC08 Hi all Would you mind if we ask SN74LV08A and SN74AHC08? What is the main difference between LV family and AHC family? It seems that there is no much difference about the supply voltage range, Switching Characteristics…
Other Parts Discussed in Thread: SN74LV08A I am using the SN74LV08A gate to protect a processor from voltage while not powered.
If there is no voltage on VCC, is it harmful for this part (SN74LV08A) to receive a voltage on one of the inputs? (1A, 2B, 2A…
Other Parts Discussed in Thread: SN74LV08A , SN74LV244A Hello,
SN74LV08(obsoluted device) has ΔICC specification as 500uA.
But SN74LV08A doesn't have ΔICC specification.
Could you please kindly let me know this reason ?
Could I have the…
Hi Michael,
As Clemens mentioned, there is an error in our search tool. I have reported this error to be fixed.
A part suggestion I can give is the SN74LV08A. This part also has over-voltage tolerant inputs. So yes, supply can be 3.3V and inputs can be…
The SN74LV08A has partial power-down (I off ) protection. Its absolute maximum ratings show that you can apply up to 7 V to an output in the power-off state, i.e., it's high impedance.
The SN74LVC08A does not have I off . The absolute maximum rating for…
Other Parts Discussed in Thread: SN74LV08A Hello,
this is my very first question.
Referring to the RS-485 Bidirectional Fan-Out Hub With Automatic Direction Control Reference Design, I would like to know why the R outputs of the 4 RS-485 transceivers are…
Other Parts Discussed in Thread: SN74LV08A-Q1 , SN74AHC08 , SN74LV8151 , SN74LVC3G17 , SN65HVD33 , SN74AHC08-Q1 , SN74AHC08-EP Automotive Quadruple 2-Input Positive-AND Gate with Input Tolerant
Hi, My customer is looking for a quadruple 2-Input Positive-AND Gate…
Hello,
I got another question. I recommended SN74LV08A-Q1, but the customer uses 1.8V which isn't supported by that. Therefore they can't use SN74LV08A. The customer found the output was forced 1.8V for 10ms - 15ms before power up when it still…