Part Number: SN74LV14A We plan to change the constant of the damping resistance at the output destination on the current board. As the output current increases, the peak current flows about 44 mA (1 μ or less) in a period of 10 to 20 μ. (There is…
Part Number: SN74LV14A Hi,
In the data sheet, the output current of SN74LV14A is 25mA per output, and it is necessary to use the entire IC so that the output current does not exceed 50mA.
When using the power supply voltage Vcc=4.5V to 5.5V, the maximum…
Part Number: SN74LV14A Hi team,
Could you please elaborate on the following marking changes due to PCN?
My customers do not understand what ECAT value G4 and unit ID coordinate mean.
Regards,
Part Number: SN74LV14A Other Parts Discussed in Thread: SN74LXC8T245 We are trying to change the good parts from the model currently under development to the non-inverting Schmitt trigger. If you search on the web page, there are 3 elements and 3-state…
Part Number: SN74LV14A Other Parts Discussed in Thread: SN74HCS14 , Hi team,
In the datasheet, only maximum value is soecified for VT+(Positive-going threshold) and minimum value is specified for VT– (Negative-going threshold).
Is it possible for you…
Part Number: SN74LV14A Other Parts Discussed in Thread: SN74LV540A , TPS3840 , TLV810E Hi Expert,
SN74LV14A Minimum Vcc is 2V.
Will it be indefinite output at less than 2V Vcc during system shutdown?
If it will be High output, they cannot use this device…
Part Number: SN74LV14A Hi team,
For how long will the device latch up if a voltage in excess of the absolute maximum rating is input? Will it latch up even for a moment?
Sincerely. Ryu
Part Number: SN74LV14A-EP Hi,
Good Day.
Could customer use SN74LV14AMPWREP instead of SN74LVU04AQPWRG4Q1? His application is only invert the TTL signaling at the inputs and nothing more than that? If the Schmitt trigger could be utilized as only invertor…