Part Number: SN74LV165A hello ,ti
now, i want use SN74LV165A chip to finish related function.
can you send me the sample code,so that i can use this chip faster and batter。
thank you very much。
my mail is:fanzhongtao@yuankunxh.com
Part Number: SN74LV165A Dear Team,
My customer would like to use SN74LV165A to support OCP 3.0 Scan Chain as below figure.
Now they provide 3.3V Vcc power to SN74LV165A and would like to use 12.5Mhz clock frequency for CLK pin.
But the spec shows that…
Part Number: SN74LV165A Hi team,
My customer is using SN74LV165A now. The schematic is below, SER and E F G H are not used here. Whether they can connect the signal together and pull up with one resistor. Thanks. It should be ok from my point of view.
Part Number: SN74LV165A Hi team,
whether the device can stand input -1.52v for 2ns? Does it have risks? How we can decide the voltage and time can stand of the SN74LV165A? Thanks.
Part Number: SN74LV165A Hi, team,
My customer uses SN74LV165A in their system. They have concern on below CLK input.
Please refer to below different CLK waveforms and check whether these are okay for SN74LV165A CLK.
Thanks.
Johnny
Part Number: SN74LV165A Hi team,
I can't find the maximum working frequency in the datasheet.
Can I calculate the maximum working frequency according to the pulse of clk? as below:
So the maximum clock frequency is 1/(2*7ns)
please help to confirm…
Part Number: SN74HC165 Other Parts Discussed in Thread: SN74HCS165 , SN74LV165A , CD74HC165 , SN74HCS165-Q1 Is there p2p compatible one with new process as the Lead time of old one is not good? Pls recommend . Thanks