Part Number: SN74LV1T125 Other Parts Discussed in Thread: SN74LVC2T45 , SN74AHC1G125 , TXS0101 , TXB0101
Hi Team,
Our customer is looking for a single +1.8V to +5V unidirectional voltage translator with tristate output. I have checked our product lines but…
Part Number: SN74LV1T125 Hi Team, Could you help us confirm the thermal resistance, particularly RθJC (junction-to-case) for SN74LV1T125 (DCK package)? Thanks in advance! Kind Regards, Jejomar
Part Number: SN74LV4T125 Other Parts Discussed in Thread: SN74LV1T125 Hello
On both the SN74LV4T125 and the SN74LV1T125, we see the Ii for the A side has current characteristics of 1uA;
do you have the maximum input current characteristics for the 3-state…
Part Number: SN74LV1T125 Other Parts Discussed in Thread: SN74AUP1G125 , SN74AUC1G125 , SN74AUC1G17 Is there any direct replacement for the SN74LV1T125 with VCC input of 1.6V?
Part Number: SN74LV1T125 Other Parts Discussed in Thread: SN74AHCT1G125 , 2N7001T , SN74AUP1T34 Hi Team,
currently my customer is using SN74LV1T125 in SC70 package (2 x 2.1mm footprint). However, this will be too big for their new project and they are looking…
Part Number: SN74AXC1T45 Other Parts Discussed in Thread: SN74LV1T125 , I usually do 1.8V to 3.3V level shift using SN74LV1T125. I find there is a direction-controlled version, SN74AXC1T45. I wonder what's the benefit to use it, except the controllable…
Part Number: SN74LVC1G34 Other Parts Discussed in Thread: SN74LV1T125 , SN74AHC1G125 Hi there,
I would like to use the SN74LVC1G34 between 2 devices which communicate via UART (3.3V).
The devices will be separated by a long cable of 5 - 10 m and the max…
Part Number: SN74LV1T125 Other Parts Discussed in Thread: SN74AHCT1G125 , , TXB0102 , TXB0104 Hi there,
I would to use this device as an interface between a 3.3V CMOS device and a 5V TTL device.
The communication between the devices is UART (unidirectional…
Part Number: SN74LV1T125 Other Parts Discussed in Thread: SN74AHCT1G125 , SN74LVC1G125 Hi
We are looking for a pin to pin, (drop and replace) replacement for the SN74LV1T125 OE buffer.
It is a " Must" that the Vin_low min of the replacement is…
Part Number: SN74LV1T125 HI
Quick question.
Could you please let me know the /OE pin termination in case of unused the output disable function?
it can connect to GND directly, or , It is needed any pull down resistor? (if pulldown resistor is required…