Part Number: SN74LV1T34 Hello,
I am using the above part number level shifter to downshift a 5V TTL signal to a 3.3V signal. I've broken a few of these chips, but when I measure the input and output lines I do not see anything happening that should be…
Part Number: SN74LV1T34 Hi,
I'm looking for a replacement part for 74AUP1T34DCK and the TI SN74LV1T34 looks to be suitable. Since the 74AUP1T34 features an additional VCC pin for the input circuit of the chip (pin 1) and I do not want to redesign the…
Part Number: SN74LV1T34 Other Parts Discussed in Thread: SN74AUP1T17 Hi Experts,
My input signal with a low 17V/s slew rate for SN74LV1T34, does it will work normal?
Thanks!
Best Regards,
Xing
Part Number: SN74LV1T34 Hi Sir,
My customer would like design SN74LV1T34DCKR and would like to know the thermal information.
Would you please review table and provide feedback? Customer also request Thermal model PDML. Please advise.
Thermal…
Part Number: SN74LV1T34 Other Parts Discussed in Thread: SN74LVC244A Hi TI Team,
I'm trying to control 4 brushless motor using a PWM signal from Raspberry Pi. The motor controller is ATMEGA328P.
I'm using SN74LV1T34 to convert 5V PWM to 3.3V PWM. In…
Part Number: SN74LV1T34 Hi Team,
There is a good new that we DIN TI product!
Customer is looking for the replacement of SN74LV1T34DCKR (P2P would be better )
Please help suggest TI solution, THX
Now SN74LV1T34DCKR is out of stock , so customer need …
Part Number: SN74LV1T34 Other Parts Discussed in Thread: SN74LVC1G34 , SN74LV1T125 Hello,
I am currently using the SN74LV1T34 (DCK package) to shift a 3.3V PWM signal of a few MHz to a 4.096 level signal. This is then just low pass filter averaged and…
Part Number: SN74LV1T34 Other Parts Discussed in Thread: SN74LVC1T45-Q1 , SN74AUP1T34-Q1 , SN74AHCT1G125-Q1 Hi team,
Do we have auto grade version for SN74LV1T34?
By the way, could we use sn74lvc1t45-q1 to replace it?
Thanks.
Part Number: SN74LV1T34 Hi,
I want to use this component to detect a 5V or 3.3V voltage and provide this detection information to an 1.8V interface controller (a FPGA).
Is this component can be used like this if i set the VCC to 1.8V ?
Reading the datasheet…