Hi Atsushi,
If phase comparator 2 is being used, then two consecutive COMP_IN rising edges would cause phase comparator 2 to down-count twice and set PC2_out low, indicating that the COMP_IN frequency is faster than SIG_IN. Similarly, if there are two…
Part Number: SN74LV4046A New to using a PLL, but have a circuit that converts 30Hz square wave to 12.288 MHz
We have fine-tuned the circuit, but still have 20-40uS jitter between reference (SIN) and CIN.
Ideas to reduce jitter? Better clock gen IC options…
Part Number: SN74LV4046A Other Parts Discussed in Thread: LM3881 Hi,
I have a customer who wants to find a simple delay chip, such as input a high level at 0 time, this chip will output the signal after 20ms delay, and it needs 3.3V power supply, please…
Part Number: SN74LV4046A Hello, when I compare PC2 Average Output voltage vs Input Phase Difference Characteristic, I obtain with my mockup, to the one in the datasheet, I have a negative slope instead of a positive slope (while PC1 and PC3 have a positive…
Part Number: SN74LV4046A Other Parts Discussed in Thread: CDCE913 Hi,
Is it possible to narrow down the frequency lock range to 118 – 125 kHz?
I see that Resistor R1 and capacitor C1 determine the frequency range of the VCO but cant find much details…
Part Number: SN74LV4046A Other Parts Discussed in Thread: CD4046B We had earlier based our design on CD4046BE with the chip operating at 5 volts. It was recommended by TI Guru to replace it with SN74LV4046A to achieve better locking. I was going through…
Part Number: SN74LV4046A Hi All, What is the temp range for SN74LV4046A? The product sheet and most of the datasheet says 85C max.
Page 1 and 11 of datasheet says 125C.
Thank you
Part Number: CD74HC4046A Other Parts Discussed in Thread: SN74LV4046A , CD4046B Hi team,
I'm looking to replace the HEF4046B with either the CD74HC4046A or SN74LV4046A. They seem to be pin-to-pin options, but there's a difference with regards to pin…
Part Number: SN74LV4046A Other Parts Discussed in Thread: CD74HC4017 , , CD4046B , CD74HC4046A I am attempting to use a SN74LV4046A PLL coupled with 4x CD74HC4017 counters to take a 0-4Hz input signal and boost that to a 0-10kHz range output. I have had…