Part Number: SN74LV74A Other Parts Discussed in Thread: SN74HCS74 Hi Team
Now customer are using SN74LV74APWR , Is there next gen of SN74LV74A which has better size and the same function? also care about power consumption
Thanks!
Part Number: SN74LV74A Hi,
My customer wants to calculate VOH under conditions not listed in the datasheet. and customer believes that once the impedance is known, it can be calculated.
My impedance calculation is ”Zo =(V㏄ – Voh min)/Ioh”.…
Part Number: SN74LV74A Other Parts Discussed in Thread: SN74LVC2G07 Hi Team,
The customer is using SN74LV74A, Open-drain output is required in the system configuration.
1. Can I use SN74LV74A Open-Drain Output?
2. If SN74LV74A is not open-drain output…
Part Number: SN74LV74A Hi Team,
Can you please help me on storage temperature and operating free-air temperature for SN74LV74ARGYR.
What is junction temperature of SN74LV74ARGYR?
Part Number: SN74LV74A Hi,
He wants to add capacitor between /Q pin and /CLR pin to reduce noise.
On normal condition, /CLR pin is High and /Q pin is Low. However if status is illegal, both pins are opposite and he has to select capacitor value Not to…
Part Number: SN74LV74A Other Parts Discussed in Thread: SN74HCS74 Hi Team,
I think SN74LV74A will enter unstable when PRE = CLR = H at start up. To avoid this, I would like to add some delay circuit at CLR pin.
- Is my understanding correct?
- What is…
Part Number: SN74LV74A Other Parts Discussed in Thread: SN74LVC1G34 Hi all Would you mind if we ask SN74LV74A? How much is output current in case of short time rating(10ms~50ms)? The datasheet shows continuous output current with /sec level. If you have these…