Part Number: SN74LVC125A Other Parts Discussed in Thread: LSF0108 Hi,
I have a cascaded buffering scheme for SPI chip select which flows as shown below,
Micro Controller --> 1x SN74LVC125A --> 8 x 74HC154 (Demux) -->1x LSF0108 --> Destination…
Part Number: SN74LVC125A Other Parts Discussed in Thread: SN74LVC1G125 , SN74LVC07A , SN74LVC2G125 Hello TI Team,
the data sheet of the SN74LVC125A states that the maximum voltage at the output is Vo VCC+0.5V.
It further states "The input and output negative…
Part Number: SN74LVC125A CS1629089: RN PCU_QC Buffer_SN74LVC125ADT_ESD_Diode on the OE# pin(Pin 1,4)
Hi,
Project Name : Renault PCU
TI part Number : SN74LVC125ADT
We are using SN74LVC125ADT buffer in our RN PCU project.
SCH attached for your review…
Part Number: SN74LVC125A-Q1 Other Parts Discussed in Thread: SN74LVC125A Hi,
The OE pull up resistor is determined by SN74LVC125A OE port sink current, please share the maximum value of the sink current or the typ pull up resistor value.
When maximum sink…
Part Number: SN74LVC125A Hello ,
I am using SN74LVC125A as buffer in between the controller and the transistor switching circuitry. I have four channel of section where need to drive two transistor on and off. These all 8 transistor need to drive from…
Part Number: SN74LVC125A If I use SN74LVC125A for buffers for test probes, please provide the Dynamic currents Icc (@Vcc=3.3V) at the rates: 5MHz,10MHz, 40 MHz and 80MHz.
Many thanks
Part Number: SN74LVC125A Other Parts Discussed in Thread: SN74LV125A , SN74LVC2G125 , Does anyone have experience using this chip where the output pin is connected to 5V, only when not driving? If the current can be limited using a resistor, is there any…
Part Number: SN74LVC125A what will be the output voltage of each pin if the IC is powered by 3.3V.? In datasheet, it is recommended that it will give Vcc output. Has anyone checked it.