Part Number: SN74LVC126A We'd like to use SN74LVC126 3-state Logic to control the transistor (NPN and PNP). As i know, the output of this logic should be push-pull topology, correct? if this is a case, why the IOH (High Level output Current) is negative…
Part Number: SN74LVC126A Dear Sir:
Regarding the SN74LVC126ARGYR for BT UART application.
Please check the schematic connection whether it is OK and reply us ASAP.
Thanks a lot.
B.R
Vincent
Module
U201 SN74LVC126ARGYR
U201 SN74LVC126ARGYR
In…
Part Number: SN74LVC126A Other Parts Discussed in Thread: SN74LV126A Hi Team,
Can you please help us with our customer inquiry below?
My concern is regarding the datasheet for the SN74LVC126A, attached, and how it used in circuit.
In the absolute maximum…
Part Number: SN74LVC126A-Q1 Other Parts Discussed in Thread: SN74LVC125A-Q1 Hi team,
Here is request from my customer shown below. I want to recommend the SN74LVC126A-Q1.
Could you please confirm following questions:
1.Do you have better recommend…
Part Number: SN74LVC126A-Q1 Hi team,
The customers want to use the SN74LVC126A-Q1, but the orderable number is different shown in datasheet and ti.com.
In ti.com, the SN74LVC126A-Q1 in the package of TSSOP-14 is CLVC126AQPWRG4Q1 shown below.
In…
Part Number: SN74LVC126A From the datasheet, it mentioned to ensure the high-impedance state during power up and power down, OE must be tied to GND through a pulldown resistor. The minimum value of the resistor is determined by the current-sourcing capability…
Part Number: SN74LVC126A Other Parts Discussed in Thread: SN74LVC541A In my application there is a case that the outputs of two SN74LVC126As are tied together directly, to drive a common destination. No serial damping resistors are allowed in between as…
Part Number: SN74LVC126A Hi Team
My customer find it doesn't work when using 6MHz UART data, but It can support 3MHz UART data. I have checked datasheet and it mentioned that SN74LVC126A could support 100MHz application. Can you double check whether SN74LVC126A…
Part Number: SN74LVC126A I have a question concerning the SN74LVC126A quadruple bus buffer gate.
I’d like the enable all four of the buffers for this part as well as three more of these IC’s.
Can you tell me what the are for these devices…
Part Number: SN74LVC126A Other Parts Discussed in Thread: SN74LV126A Hello,
This might be basic, but could you tell me the device internal circuit.
Is there a clamp diode or any resistors on the output pin?
When we tried live insertion using LVC126A…