Part Number: SN74LVC126A From the datasheet, it mentioned to ensure the high-impedance state during power up and power down, OE must be tied to GND through a pulldown resistor. The minimum value of the resistor is determined by the current-sourcing capability…
Part Number: SN74LVC126A I'm looking for a data buffer to handle a parallel video data bus running up to 300MHz at Vcc = 3.3V. Can anyone suggest a suitable device? Anything from 1 to 10-channel would do!
Thanks
Part Number: SN74LVC126A I have a question concerning the SN74LVC126A quadruple bus buffer gate.
I’d like the enable all four of the buffers for this part as well as three more of these IC’s.
Can you tell me what the are for these devices?
It…
Part Number: SN74LVC126A-Q1 Other Parts Discussed in Thread: SN74LVC125A-Q1 Hi team,
Here is request from my customer shown below. I want to recommend the SN74LVC126A-Q1.
Could you please confirm following questions:
1.Do you have better recommend…
Part Number: SN74LVC126A Other Parts Discussed in Thread: SN74LV126A Hello,
This might be basic, but could you tell me the device internal circuit.
Is there a clamp diode or any resistors on the output pin?
When we tried live insertion using…
Part Number: SN74LVC126A-Q1 Hi team,
The customers want to use the SN74LVC126A-Q1, but the orderable number is different shown in datasheet and ti.com.
In ti.com, the SN74LVC126A-Q1 in the package of TSSOP-14 is CLVC126AQPWRG4Q1 shown below.
In…
Part Number: SN74LVC126A-Q1 Other Parts Discussed in Thread: SN74LVC1G08-Q1 Hello,
Kindly review the attached design using SN74LVC126AQPWRQ1 Thanks,
Melbin
SN74LVC126AQPWRQ1_SCH_28DEC2020.pdf
Part Number: SN74LVC126A Hello
Does anyone may point me to the footprint for the SN74LVC126APW? Only the package is defined. The recommended footprint is not. Is there any recommended one from TI?
Thanks