Part Number: SN74LVC16373A Team,
My customer has the following request:
Trying to get a “Absolute Maximum Operating Temperature” for SN74LVC16373ADGVR in TSSOP 48 package (See spra953C for definition). Datasheet gives only Maximum Operating…
Hello,
- Junction Temperature Max (Tj Max) – This information can be found in the absolute maximum table of the datasheet.
- Typical Power, (Pd typ) – This can be found in the electrical characteristics section of the datasheet.
- Maximum Power (Pd…
Ivan,
That would appear to be correct to me. The only exception being that the the SN74LVC16373A and SN74LVC138A seem to only be rated to voltages greater than 3.6V in the absolute maximum ratings tables - so some conditions of the Electrical Characteristics…
Other Parts Discussed in Thread: SN74LVC16373A , SN74AVCH8T245 , SN74AVC16T245 We are using the below latch and level translators in our design
1. SN74LVC16373A - Latch- OE pins are recommended to be pulled high with VCC
2. SN74AVCH8T245 & SN74AVC16T245…
Other Parts Discussed in Thread: SN74LVC16373A Hi,
I have a question about the part of NOR Flash which is on the application board of AM3517EVM.
I saw following TI wiki: http://processors.wiki.ti.com/index.php/AM3715/03_GPMC_Subsystem#16-bit_NOR_with_external_latch…
Other Parts Discussed in Thread: SN74LVC16373A , OMAP3503 Hi,
we use a OMAP3503 with a Numonyx Axcell P30-65nm, 1-Gbit flash. The lower 16 address lines are demultiplexed with a SN74LVC16373A latch. Our problem are sporadic writing problems to flash. Once…
Hi,
I have given the schematic a thought, and it looks like the circuit is wrong !
It needs an inverter on the latch gate:
the SN74LVC16373A is transparent when LE is high.
From the Figure 6-12 of the OMAP3530 datasheet (Async write, muxed ad/dat…
Select this link to see answers to common questions, detailed use case implementations, and part recommendations for logic and voltage translation devices. .
Top Logic and Voltage…