Part Number: SN74LVC1G07 Other Parts Discussed in Thread: SN74LVC1G06 , , SN74LVC1G17 , SN74LVC1G14 , SN74LVC1G99
SN74LVC1G06 is inverter with "Schmitt Trigger Action on All Ports".
SN74LVC1G07 is buffer but does not say Schmitt trigger.
Is this…
Part Number: DP83869HM Other Parts Discussed in Thread: SN74LVC1G06 , SN74LVC3G06 , SN74LVC3G07 , SN74LVC1G07 , SN74LVC2G06 , SN74LVC2G07 Hi,
I work with vddio of 1.8V.
pls. advise who to drive the phy leds because direct drive is not working when you have…
Hi Shinji,
I did a bit more searching around E2E, and I think that this part is not actually a Schmitt trigger input, because if it was then in the electrical characteristics section of the D/S there would be a V_t+ and V_t- spec given.
https://e2e.ti…
Regarding the subject line part, I noticed in the datasheet that the part specifies the low level output current and voltage in the datasheet as shown below:
The datasheet does not specify the high level output current and voltage. On the main TI…
Part Number: ADS8422 Other Parts Discussed in Thread: SN74LVC1G06 , I need to connect together 32 ADS84221 (pin 36 BUSY). I would like to have the exact specifications of this output.
These 32 pins will be connected together and connected to one pin of…