Part Number: SN74LVC1G3157 Hi,
Need to validate the capacitance ON - OFF state measurement of the above-mentioned CMOS SPDT Switch.
Please recommend the test procedure and any test equipment needed to test for the same.
Part Number: SN74LVC1G3157-Q1 Hi team,
Would you pls help share how to evaluate the power dissipation and thermal performance of SN74LVC1G3157-Q1 under below condition? Customer is concerning since our thermal resistance on datasheet is large.
Supply…
Part Number: SN74LVC1G3157 Other Parts Discussed in Thread: TS5A63157 , TS5A3157 , , TS5A3159A Hi,
If VCC is no supply and pin4 (A) is applied 3.3V, will there voltage leakage to pin1, pin3, pin5 or/and pin6?
Thanks and Best regards,
Tiger
Part Number: SN74LVC1G3157 Hello,
We are designing with the SN74LVC1G3157 and had a question from the datasheet (copied below).
Could you please share what parameters would typically cause the change of supply current ΔIcc?
Does this change typically…
Part Number: SN74LVC1G3157 Other Parts Discussed in Thread: TS5A63157
Hi Team,
We have 2 custom made PCBs A and B.
PCB A has this part 'SN74LVC1G3157DBVR' used to pass a 3V line to a OPAMP circuit.
The control for 'SN74LVC1G3157DBVR' is from…
Part Number: SN74LVC1G3157 I have a somewhat specific question about the implementation of clamping diodes:
From the fact that in the datasheet there is a pos/neg max. current specification (50mA) for the "IO port diode current" I conclude that there…
Part Number: SN74LVC1G3157 Other Parts Discussed in Thread: TS5A63157 , TS5A3160 你好,ti专家
SN74LVC1G3157在VCC没有上电的情况下,A端口是否能可以有电压。
按datasheet的9.2.1描述,需要等待到VCC建立后才可以加信号,我们的应用是 SN74LVC1G3157在目标电路板的接口上,外加的信号由其他电路板提供,不受SN74LVC1G3157目标板控制。