Other Parts Discussed in Thread: SN74LVC1G3157-Q1 Dear, All
There is a question about S-pin of SN74LVC1G3157-Q1. - Is pull-up resistor or pull-down resistor had by S-pin built-in?
This is because I'd like to know the state of the device when soldering…
Part Number: TCAN1146-Q1 Other Parts Discussed in Thread: TMUX1248 , SN74LVC1G3157-Q1
Hi,
In one of our application design, using the TCAN1146-Q1 below is details. Pls suggest me MUX/DEMUX part used in design for SDO/nINT.
Thank you.
Regards…
Part Number: TCAN1146-Q1 Other Parts Discussed in Thread: SN74LVC1G3157-Q1 , Hi TI Team,
We are using TCAN11446, we want to use RXD pin as wake up source for processor to be woken up.
In sleep mode of TCAN1146 VCC & VIO are not available, we are turning…
Part Number: SN74LVC1G3157 Other Parts Discussed in Thread: SN74LVC1G17-Q1 e2e,
I am now evaluating SN74LVC1G3157-Q1, and have 2 questions for this device:
1. Is the measuring range of Input transition rise or fall rate spec from VIH to VIL? …
"1.8 V logic" describes only the control inputs.
I am not aware of any device that combines muxing and level shifting.
I'd suggest to combine a mux like the SN74LVC1G97-Q1 or SN74LVC1G3157-Q1 with a separate level shifter like the SN74LVC1T45-Q1.
1% at 200kHz should have maximum transition time 50ns on the calculation, and TS5A3159-Q1 is slightly over than the 50ns, so this is not proper, is this correct?
The TS5A23157-Q1 or SN74LVC1G3157-Q1 is fast enough, because the ton and toff is about…
Hi, Louise:
Customer is looking for SN74LVC1G3157-Q1 since it has very low price compared to TS5A3159-Q1. Do you have any comments for the difference between SN74LVC1G3157-Q1 and TS5A3159-Q1. We know the Ron of SN74LVC1G3157-Q1 is larger which is…
Hi Stephen,
Thank you for your reply.
Since I need Q100 device, csdxxx cannot be used.
Does the analog switch below also work?
https://www.ti.com/product/SN74LVC1G3157-Q1
https://www.ti.com/product/TMUX1309-Q1
I have a question about the…
TI offers a wide range of automotive rated signal switches and multiplexers. This flyer is a quick snapshot of some of our most popular devices.
A downloadable version of the flyer with links to product folders and relevant content can be found…