Part Number: SN74LVC1G66 Dear Team,
For SN74LVC1G66DBVR, Please help to check why it's current marking is C66J, while our datasheet marking is C665/C66R/C66T?
brs
Allen
Part Number: SN74LVC1G66 Hi team,
My customer requested IBIS model of SN74LVC1G66DSF. Could you please provide the data?
If we don't have, how the customer do for simulation?
Regards,
Yoshi
Part Number: SN74LVC1G66 Hi
I need to pass 1.2V POD12 reset output from one of the controller to memory chips (once controller came out of its RESET).
planning to use 74LVC1G66 with Control pin controlled by Controller's reset signal(1.8V level). …
Part Number: SN74LVC1G66
Hi Experts,
We are going to use an analog switch to connect two MCU's IO ports. Due to some reason, there might be a chance that both MCU ports output and the short current flows as below.
This current is defined as abs…
Part Number: SN74LVC1G66 Other Parts Discussed in Thread: DXP Hi team,
I need to use U ltra Librarian software to convert CAD file to altium designer file for SN74LVC1G66.
After I get the UL_Form.dfm, UL_Form.pas, UL_Import.pas and UL_Import.prjScr file…
Part Number: SN74LVC1G66 Other Parts Discussed in Thread: SN74CB3Q3305
Hi team,
I want to use SN74LVC1G66. VCC is 3.3V. The datasheet shows the I/O port voltage range is from 0 to VCC.
Q1:I want to confirm if the input voltage exceeds 3.3V, can the input…
Part Number: SN74LVC1G66 Hi team,
For the frequency response of SN74LVC1G66, in our datasheet, there is only type value. show as below:
Customer want to know the minimum value of the frequency response?
Can you help to provide the it?
Lace…
Part Number: SN74LVC1G66 Hi Team,
Customer is using SN74LVC1G66 to transfer I2C signal. The pull-up supply of I2C is 3.3V . The power supply of switch is 5V, which means that the high-level input voltage is 3.5V, higher than 3.3V.
Can SN74LVC1G66 still…