Part Number: SN74LVC1G79 Tool/software: Hello,
During the customer's use of SN74LVC1G79, a large number of devices experienced VCC and GND short circuits. The quantity is approximately 800 pieces. Previously used without any short circuit issues. The…
Part Number: SN74LVC1G79 Other Parts Discussed in Thread: SN74LVC1G374 Tool/software: Hi team,
My customer is using SN74LVC1G79 and met issue during the power on.
Magenta channel 4 is the D input signal of the trigger, yellow channel 1 is the 5V…
Part Number: SN74LVC1G79-Q1 Hi experts,
These parts have MSL level marked as NC, while the same part# of another DC has the detailed information.
These were from TI Franchise. Datasheet shows that the MSL of this item is Level 2.
What's the meaning…
Part Number: SN74LVC1G79 Other Parts Discussed in Thread: SN74HCS74 Does this part (likewise, the "LVC1G80, 'LVC2G79 and 'LVC2G80) have any type of internal power-on reset that guarantees the start-up state of the Q (or /Q) output? Or do they just come…
Part Number: SN74LVC1G80 Other Parts Discussed in Thread: SN74LVC1G79 , , SN74HCS74 My customer want to default output low level,but when use SN74LVC1G80,it default output low level.Can I use SN74LVC1G79 to output low level by default?
Blow is the customer…
I'm afraid we only have the data that is currently in the datasheet. Since the output impedance doesn't change much over operation, you should be able to get a good estimate with the existing values.
Part Number: SN74LVC1G79 Please let us know if the Part Number SN74LVC1G79DBVTE4 is Active/Obsolete/Invalid.
If Active, provide us the YTEOL(Years to End of Life Information).
If Obsolete, provide us the supporting documents i.e, EOL notice, PCN along…
Part Number: SN74LVC1G79 Hi Expert
When using SN74LVC1G79 (VCC is 5V, D is pulled up to 5V via a resistor), during power up, before CLK high logic come, the output already output high.
To check more, Pin D and Pin CLK are both floated, then it is…
Part Number: SN74LVC1G79-Q1 Hi Team
What does the ΔICC represent in the datasheet?
What's the difference with ICC?
How should ΔICC be applied when calculating the total current consumption of an IC?
Thank you
Hello,
Unfortunately we do not have any characterization data for the jitter level of this device.
Please note that we are trying to ensure that all posts are answered. With any new posts, we will be sure answer in a timely manner so that no posts…