Part Number: SN74LVC1G97-Q1 Team,
My customer has the following question:
I have a question regarding the propagation delay specification for the Texas Instruments P/N SN74LVC1G97QDCKRQ1 configurable logic gate. The propagation delay is specified to…
Part Number: SN74LVC1G97-Q1 We’re starting verification that all semiconductor components SN74LVC1G97-Q1 have ISO 26262 (Functional safety) according to attached GS95033-1.
Please review and confirm for below parts.
Thanks
Evgeny
Hi Clemens,
thanks for the fast response. I was not aware of SN74LVC1G97-Q1 and that you can configure it as OR gate.
Thanks for the recommendation!
Michael
Part Number: SN74LVC1G97-Q1 Looking at the SN74LVC1G97-Q1 logic gate. Datasheet states absolute max voltage on logic inputs is 6.5V and appears to be independent of Vcc. I'm looking for confirmation that this Vi limit is in fact independent of the device…
Part Number: SN74AHC1G08 Other Parts Discussed in Thread: SN74AHCT1G08 , , SN74LVC7001A , SN74HCS08 , SN74LVC1G97 , SN74LVC1G08 Tool/software: Hello guys,
One of my customers is considering using SN74AHC1G08 or SN74AHCT1G08 for their new products.
At this…
Part Number: SN74LVC1G97 Other Parts Discussed in Thread: SN74LVC1G32-Q1 Hello, please ask if the SN74LVC1G97QDCKRQ1 can be replaced by a two-input or gate logic IC, and is there a recommended model
AC and LVC are entirely different (from SCLA013 ):
As for the buffers, their material content reports show that the weight of the die in the 2G devices is neither the same nor double that of the 1G devices.
If reducing the number of gate types is worthwhile…
Part Number: SN74AHC1G08 Other Parts Discussed in Thread: SN74LVC1G97-Q1 , SN74HCS08-Q1 Hi team,
Does TI have alternative option with Schmitt-trigger input and DRL package similar to SN74AHC1G08? I've found SN74HCS08-Q1 or SN74LVC1G97-Q1 has Schmitt…
"1.8 V logic" describes only the control inputs.
I am not aware of any device that combines muxing and level shifting.
I'd suggest to combine a mux like the SN74LVC1G97-Q1 or SN74LVC1G3157-Q1 with a separate level shifter like the SN74LVC1T45…