Part Number: SN74AHCT02 Other Parts Discussed in Thread: SN74HCS02 , SN74LVC1G98 , SN74AHCT541 Dear Team,
Our customer is considering to use SN74AHCT02.
They confirmed input Tr/Tf of SN74AHCT02. As this result, Tr was 56.3ns between 0.8V to 2.0V. Tf was 75…
Please note that Y1/Y2 are not outputs and have no drive strength on their own. They are either connected to COM or disconnected, so their voltage is either 5 V or floating (undefined). It is not possible the measure the voltage of a floating pin. You…
See [FAQ] What is the default output of a latched device? (Flip-Flop, latch, register)
Apparently, you want a circuit that powers up with the output at 0, and permanently switches to 1 at the first rising edge.
This can be done with a flip-flop like the…
Hi Arjun,
The SN74LVC2G125 has an output-enable. So when the enable input goes high, the output (which will be the LI and HI input) will go to high-impedance. You maybe could use it if you put a pull-down resistor on the output so that it would then be…
Part Number: SN74LV1T125 Other Parts Discussed in Thread: SN74LVC1G57 , SN74AHC1G125 , SN74LVC1G97 , SN74LVC1G99 , SN74LVC1G98 , SN74LVC1G125 , , SN74LVC1G58 , SN74LV1T34 , SN74AHCT1G125 , SN74LVC1T45 Hi, I have a micro-controller with only 3.3V tolerant inputs…
Other Parts Discussed in Thread: SN74LVC1G38 , SN74LVC1G00 , SN74AHC1G00 , SN74LVC1G97 , SN74LVC1G98 Hi Sir,
Sorry to bother you.
We would like confirm if no VCC, what is the SN74LVC1G38 output state??
Because we have use SN74LVC1G00, Looks the output is pull…
Other Parts Discussed in Thread: SN74AHC1G00 , SN74AHC132 , SN74LVC1G98 Hello!
On SN74AHC1G00 product page http://www.ti.com/product/SN74AHC1G00/description
specified, that
" Features ....... Schmitt Trigger Action at All Inputs Makes the Circuit Tolerant…
Select this link to see answers to common questions, detailed use case implementations, and part recommendations for logic and voltage translation devices. .
Top Logic and Voltage…