Part Number: SN74LVC1GU04 Other Parts Discussed in Thread: SN74LVC1GX04 Tool/software: Hi Team,
This is Jayden, may I ask the max bandwidth this device can support? 100M? I can't find this in datasheet.
Brs
Jayden
Part Number: SN74LVC1GU04 Other Parts Discussed in Thread: SN74LVC1G04 , SN74LVC1G14 , Tool/software: HI Team,
Can you share tr/tf spec?
is it 10ns/V?
Thanks,
Vidya
Part Number: SN74LVC1GU04 We are using the SN74LVC1GU04 and I have a few question about it:
Can the VCC be 5V and at the input of the component the signal voltage will be 2.85V?
VOH at 3V is 2.3V (min) what is the max value ?
VOH at 2.3V is 1…
Part Number: SN74LVC1GU04 Hi Team,
Good day. I am posting this inquiry on behalf of the customer.
"What is the minimum level of VIH when VCC power supply is 2.85V?
Calculated with 'Recommended Operating Conditions' below, VIH should be 2.1375V …
Part Number: SN74LVC1GU04 Other Parts Discussed in Thread: SN74LVC1GX04 Hi, Expert
for SN74LVC1GU04 datasheet, Signals that are applied to the inputs need to have fast edge rates, as shown by Δt/Δv, but there are no specific spec for Δt/Δv, could you…
Part Number: SN74LVC1GU04 Dear TI Technical Team,
We are considering using your SN74LVC1GU04 part for analogue applications and we need to know the transconductances of both N and P transistors. Could you help us, please?
Thank you.
Yours faithfully…
Part Number: SN74LVC1GU04
I am using SN74LVC1GU04 IC in above circuit. the mosfet gate resistance is 10ohm. at the time of turn on mosfet gate will draw a peak current = 5/10 = 0.5A from the NOT gate output pin, whether this will destroy the output…
Part Number: SN74LVC1GU04 Hello guys,
One of my customers is going to use SN74LVC1GU04YZV for thier new products.
So they need to get the device footprint to make PCB.
Could you please tell me how to get the device footprint data with PDF format…
Part Number: SN74LVC1GU04 Hi all,
Customer want to know whether we have input and output resistor of SN74LVC1GU04, which will influence the output driver current and input impedence match.
Below is the block diagram of 74LVC1GU04 and 74AUP1GU04
…
Part Number: SN74LVC1GU04 Hi,
I'm attempting to run a simple HSPICE simulation with this part, but can't checkout a "TI" feature on my license. It's the first time i see such an error. I read somewhere it's because the model is Level 37 and it needs…