Part Number: SN74LVC1GU04 I was wondering if anyone can give any information with regards on how the operating temperature limits are determined for this part single hex inverter. Data sheet has a -40C to +125C operating range but I would like to use…
Part Number: SN74LVC1GU04 Other Parts Discussed in Thread: SN74LVC1G14 , LM339 Hi,
What is the gain of products in the LVC family? What about the schmitt trigger verion (sn74lvc1g14)?
I notice ~25dB at 3.3v from for the GU04 this document:
www.ti.com/.…
I appreciate your reply.
The following document states that LVC is 10ns/V (max). www.ti.com/.../scba004e.pdf
Also, in the past E2E, there are xx answers. e2e.ti.com/.../sn74lvc244a-t-v-input-transition-rise-or-fall-rate e2e.ti.com/.../sn74lvc1gu04-t-v-requirement…
Part Number: SN74LVC1GU04 Hi
The absolute maximum rating of VI of sn74lvc1gu04 shows 0.5V to 6.5V.
However, VI offers 0V to 5.5V in the recommended operating condition.
Why is the abs value of VI(min) defined 0.5V?
This device can accept VI=0V, right…
Part Number: CD4521B Other Parts Discussed in Thread: SN74LVC1GU04 , SN74LVC1G80 Hello, I was wondering if we could get some help, as we are using your CD4521B as a frequency divider, but our crystal is not oscillating for a strange reason. The Crystal…
It looks to me like you're getting a harmonic that's coming off the oscillator circuit.
My first recommendation would be to switch to an unbuffered inverter - the gain will be reduced and it should help with this. SN74LVC1GU04 is a good example…
Part Number: SN74AUC1G125 Other Parts Discussed in Thread: SN74LVC1GU04 HI Team,
Please help to confirm correct YZP package size which we marked differently in data sheet P.1 and P.19. The package length and width are different. Thanks
http://www.ti…
A Schmitt-trigger inverter should never output an analog voltage.
What is the amplitude of the input? Can you show oscilloscope traces?
An opamp without negative feedback would not result in a gain of −1.5. If you have a wrong device, I would guess it…
Hi Linda,
While the SN74LVC1G240 can be used in oscillator circuits, it is a buffered inverter and won't be as stable as an unbuffered inverter. The SN74LVC1GX04 Crystal Oscillator Driver is much better suited for driving a crystal oscillator. The SN74LVC1GX04…
Part Number: SN74LVC1GX04 Other Parts Discussed in Thread: SN74LVC1GU04 , HI,
To calculate my Load Capacitance correctly i should know the input capacitance of this IC at the X1 port. In the Data sheet i just found the Ci value and I hope that this is applies…