There is no difference between devices with and without -E4; see [FAQ] Why does a logic device's part number have an E4/G4 suffix?
However, TI has begun switching to a new design (see PCN#20200629000.1), which has some hysteresis at the inputs. This…
Hi Yaseer,
What voltage range? If it's a low voltage application I recommend looking at some devices from our AUC and AUP families:
Inverting buffers & drivers product selection | TI.com
Otherwise if you need more voltage support I'd use the LVC1GX04…
Part Number: SN74HCU04A Other Parts Discussed in Thread: SN74LVC1GX04 Hi Team,
I use SN74HCU04APWR as an oscillator, but the waveform generated at the second stage is abnormal. Do you have any suggestions? The related circuit used, the waveforms of 1Y and…
Part Number: SN74LVC1GX04 I am using the T.I. SN74LVC1GX04 in the DRL package, but am having problems with reflow soldering. The SN95/AG05 solder does not want to wet to the package leads. The DRL just floats on top of the solder. The other chip components…
Part Number: SN74LVC1GX04 Other Parts Discussed in Thread: TLV320AIC3204 Hi,
I would like to generate 12.288MHz clock using crystal. This clock is to fit into TLV320AIC3204 MCLK. In AIC3204 datasheet, I see the logic input is having CL=10pF and I=5uA.…
Other Parts Discussed in Thread: SN74LVC1GX04 Hello,
I want to generate 16MHz clock can I use this IC i.e. SN74LVC1GX04 to generate the 16MHz clock . Please let me know as soon as possible.
Thanks and Regards
Thippeswamy
Part Number: SN74LVC1GX04 Other Parts Discussed in Thread: LMK61E2
Hi,
Could you please share the jitter performance for SN74LVC1GX04 with me if you have this information ?
Best regards, Kato
The new die of the HC04 has more hysteresis at its input buffers, which improves handling of digital signals. But a crystal does not output a digital signal.
The application report tells you that a Pierce oscillator requires an unbuffered inverter, such…
Hi Clemens-san,
Thank you so much for your suggestion!
By the way, I wonder why the app note doesn't list SN74LVC1GX04 as the recommended inverter.
I recommend you to update E2E Logic FAQ for oscillator, and SCEA099.
Regards,
Itoh