Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Other Parts Discussed in Thread: SN74LVC2T45 , SN74LVC2T45-Q1 Hi,
Let me confirm about below.
When I checked datasheet of SN74LVC2T45, then spec of "ESD ratings" and "thermal information" are described.
However, I could not find these…
Part Number: SN74LVC2T45 Hello guys,
One of my customer uses SN74LVC2T45 for their current products. Also they received PCN of the device recently and they knew the device datasheet was updated. Then they found tat the updated datasheet (Document No. SCES516M…
Hi Wenting,
Wenting Wu said: What's the maximum frequency of input signal and its duty cycle which SN74LVC2G17-Q1 can accept?
This device does not have a rated maximum input frequency or duty cycle. These will both be dependent on your system much more…
Part Number: TXU0304-Q1 Other Parts Discussed in Thread: SN74LVC2T45 Hi team,
Why could we use 200Mbps data rate @ 3.3V to 5.5V level shifting in spite of signal propagation delay = 0.5~10ns?
SPI master output clock is 200MHz (come from 200Mbps), which…
Part Number: SN74LVC2T45 Dear team
The customer would like to check the number arrangement of device marking.
Form datasheet page 20. The d evice marking of SN74LVC2T45DCUR is CT2X.
1. From top of package, the number arrangement of device marking is Q3,Q1…
Part Number: TXB0104-Q1 Other Parts Discussed in Thread: SN74LVC2T45-Q1 , SN74LVC1G17-Q1 Hi team,
Can you confirm if TXB0104-Q1 is okay for SPI interface of below configuration?
Thanks,
Sam Lee
Part Number: TXB0104-Q1 Other Parts Discussed in Thread: SN74LVC2T45-Q1 Dear all,
i need to connect 2 different boards by a 40cm long cable. The communication interface is SPI.
Inside the board the voltage level is 3V3 and for transmission 5V is used…
Part Number: SN74LVC1T45-Q1 Other Parts Discussed in Thread: SN74LVC2T45-Q1 , SN74AXC1T45-Q1 , TXS0102-Q1
Dear Support Team,
We are looking for alternate part for SN74LVC1T45-Q1 with Dual bit and Dual direction selection part.
For UART design, Checking…
Part Number: SN74LVC1T45-Q1 Other Parts Discussed in Thread: SN74LVC2T45-Q1 I see the following in the SN74LVC1T45-Q1 datasheet:
A proper power-up sequence is advisable as listed in the following:
1. Connect ground before any supply voltage is applied…