Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Hi Prachi,
2) You can also consider using multiple SN74LVC2T45-Q1 device if you need few A to B and few B to A channel control.
Refer to this app note on the LVCxT devices:
www.ti.com/.../slva746.pdf
FAQ: Logic and Voltage Translation > Voltage Translators >> Current FAQ
Here are the voltage level translation device recommendations for various industry standard interfaces:
Interface
Recommended Device
3.6V Maximum
5.5V Maximum
FET R…
Itai san,
I would suggest using the SN74LVC2T45-Q1 for 5V translation. There is no internal current limit in this device, however, short to gnd would not likely damage the FPGA device as they would be isolated from the LVC device.
Please let me know…
Part Number: SN74AXC8T245 Other Parts Discussed in Thread: SN74LVC8T245 , , SN74LVC2T45 , SN74LVC16T245 , LSF0108-Q1 , TXB0108 , LSF0108 , SN74LV4T125 , CD40109B Hey Guys,
I made a terrible mistake: I use the SN74AXC8T245PW in my design and reconfigured the VccB…
Part Number: TXS0108E-Q1 Other Parts Discussed in Thread: TLV2553 , , SN74LVC2T45 , SN74LVC1T45 Hello
I use TXS0108E-Q1 to finish spi communication between 3.3V and 5 V for driving ADC TLV2553
THis is my Schematic:
I have read the reference book :the maximum…
Other Parts Discussed in Thread: SN74AVC2T45-Q1 , SN74LVC2T45-Q1 , TXS0102-Q1 , TXS0102 , LSF0108 [ TXS0102 ] Level Translator for MDC and MDIO
Hi, Can you suggest the solution of level translating application for MDIO and MDC signals? Side-A: 3.3V Side-B: 2…
Hi,
Thanks for the quick reply. Which TI part do you suggest?
I have shortlisted these 2 in the order of preference. Am I choosing the right one?
SN74LVC2T45-Q1
SN74AVC2T245
Thanks in advance.
-Shashi.
Other Parts Discussed in Thread: SN74AVC2T245 , SN74AVC4T245 , SN74LVC2T45 Hi Team,
Our customer requests us the information of the thermal characteristic of SN74LVC2T45YXPR. Could you provide us the following two information ?
[Q1] What is Theta JC (Junction…
Quickly find solutions to common questions about voltage translation (level shifter) devices by clicking this link. This FAQ answers the most common questions asked about these devices …… ……… …
Auto-Bidirectional…