Part Number: SN74LVC4245A Hi Team,
The specs listed in table 7.1, like Io(Continuous output current)/Iok just refer to one channel, not the total channels, right? Thanks.
Best,
Stanley
Part Number: SN74LVC4245A Other Parts Discussed in Thread: SN74LVC8T245 This is a special application of SN74LVC4245A , GNDA is the ground of output signal which is 1V above input signal ground(GNDB). customer perform test and found PIN11&12 and PIN13 are…
Part Number: SN74LVC4245A Other Parts Discussed in Thread: SN74LVC8T245 Greetings,
Do we have Pspice model for this part of SN74LVC4245A?
A customer need it.
Thank u in advance.
Part Number: SN74LVC4245A Hi Team,
In my customer's application circuit, there is a condition that SN74LVC4245A's A-side is powered on, while B-side is powered down, and /OE and DIR are grounded, and all B side input signals are pulled down through a…
Part Number: SN74LVC4245A Other Parts Discussed in Thread: SN74LVC541A Dear TI Expert~
This chip SN74LVC4245A is used for serial port to receive RX level conversion, and converts 5V to 3V3, so that two devices can communicate normally.
When the master…
Part Number: SN74LVC4245A Hi team,
My customer would like to connect the DIR and /OE pin to 3.3V CMOS output from programmable logic device.
Is there any issue of this connection? Please let me know if this cause any issue.
From the datasheet, should…
Part Number: SN74LVC4245A Other Parts Discussed in Thread: SN74LVC8T245 , Hello,
I want to use 74LVC4245A for one of my project for converting 8 signals from 3.3V into 5V level.
Please find the attached image.
Can I use this for my application? Also I need…
Part Number: SN74LVC4245A Dear team,
Customer is using our SN74LVC4245A, there is a glitch above their square input voltage rising and falling edge.
So the input voltage can have a periodic over range, and the maximum input voltage is 600mV larger than following…
Part Number: SN74LVC4245A
Hello,i want to convert the signals from 3.3v given by the microcontroller to 5v to drive a lcd,but i have one servo motor and two esc(electronic speed control) who also want the signals at 5v.
I saw many voltage Translation…
Part Number: SN74LVC4245A
I have a technical question/issue about excessive overshoot and undershoot seen with using the TI SN74LVC4245APW buffer is driving the signals to an on-board module. I tried a different part (TI SN74LVC8T245PWE4) that is footprint…