Part Number: SN75ALS1177 Other Parts Discussed in Thread: SN75ALS1178 , , SN65C1168E , SN75C1168 , SN65C1168 Dear Specialists,
My customer is evaluating SN75ALS1177NS as a replacement for SN75ALS1178.
They have a question about current consumption.
I would…
Part Number: SN75ALS1177 Other Parts Discussed in Thread: SN75ALS1178 , HI Sir:
I want to confirm the below question
Does the SN75ALS1177 or the SN75ALS1178 include two transceivers and they compatible with RS422??
Thanks
Best Regards
Part Number: SN75ALS1178 Dear Specialists,
My customer is evaluating SN75ALS1178NSR(SO Package) and SN75ALS1178N(DIP package) .
They have questions, I would be grateful if you could advise.
---
Since SN75ALS1178NSR (SO Package) was not available, communication…
Part Number: SN75ALS1178 Other Parts Discussed in Thread: THVD1451 , THVD1424 , SN65HVD70 , Hello,
I am using this transceiver to send signals between a 3.3V microcontroller to a 5V differential bus.
If I provide 5V to VCC and +/-5V signals to the Recieve…
Part Number: SN75ALS1178 Hi All,
I have a question about SN75ALS1178.
What are the lower limits of absolute maximum ratings for the DE pins (pin 4, pin 12) and driver input pins (pin 9, pin 15)? Only the upper limit values are listed in the datasheet. …
Part Number: SN75ALS1178 Tool/software: What is the minimum operating voltage for SN74ALS1178? We understand the recommended operating voltage. (5V±0.25V)
Overvoltage damage would be permanent. The problem going away after some time sounds as if this is a thermal problem.
Is the chip hot? (You should be able to feel it, but be careful.)
A thermal problem would be caused by a very high power dissipation…
Part Number: SN751178 Other Parts Discussed in Thread: SN75ALS1178 , Hello Support team,
What is difference between SN751178NSR and SN75ALS1178NSR? My customer can't find SN751178NSR in market, they would like to confirm if SN75ALS1178NSR can be used…