Part Number: SN75LVCP422 Hello,
I want to know SN75LVCP422 is if it’s fully SATA compliant (verified or certified) --SATA has some strange protocols that makes me nervous. Let me know if we have any test results or SATA compliance documents that I can…
Hello,
The specified ReDriver - it is intended to be used with up to 2m SATA cable connected to HD. Can I cascade two chips to extend the length to 4m?
Jacek Kupinski
Optech.
Other Parts Discussed in Thread: SN75LVCP422 The pinout of the SN75LVCP422 is such that I'd have to roll the SATA RX pair (through some non-optimal layout) in order to connect RX+/- from the connector to the IC without inverting the bus. Is that correct…
Hi,
Are there any new regarding this design option?
We are designing a new product with similar SATA sub-system functionality.
This looks like: HOST <-> SWITCHES (SN65LVCP404) <-> REDRIVERS (SN75LVCP422) <-> discs
Hi Micheal,
more questions:
- SN75LVCP422 - previous chip we used didn't mention any ESD warnings claiming the level of +/-8kV -this chip has listed >5kV with warning of ESD sensitive device. Did you record any instances of pines being zapped?
-…
Vidhya,
What is the problem with the single PowerGood output from the TPS65400? The TPS65400 is a good part for this design. Alternately, TI has a large selection of devices that can be implemented individually. You should follow-up on the power forum…
Nanjunda,
Please see the attached presentation put together some time back by our power team. It shows an optimized solution for powering multiple K2H devices on slide 10.
6305.TI Analog Solutions for Keystone2 Family.pdf
Regards,
Senthil
Angad Shah,
Please see the attached presentation put together some time back by our power team. It shows an optimized solution for powering multiple K2H devices on slide 10.
Tom
TI Analog Solutions for Keystone2 Family.pdf