Part Number: SN75LVCP601 Hi, Team,
For below pins, is it ok to connect VDD directly or should the customer pull up by 4.7kohm? EN EQ1/2 DE1/2 DEW1/2
Best Regards, Satoshi Yone
Part Number: SN75LVCP601 We are trying to use the SN75LVCP601 on a M.2 card in a INTEL NUC computer to communicate with an external SSD.
We are able to connect one of your SN75LVCP601EVM demo boards from the INTEL NUC M.2 port as well as from the internal…
Part Number: SN75LVCP601 The sllu211.pdf shows an evaluation schematic with capacitors 0.012uF on both TX/RX lines... Is it what is recommended to use these caps on both lines? What if the other card has the capacitors as well... is it OK?"
Other Parts Discussed in Thread: SN75LVCP601 , SN65LVPE502 , DS80PCI102 Dears,
My customer asked SN75LVCP601 can support 2.5G SerDes? Thanks a lot!
BR,
Rory
Part Number: SN75LVCP600 Other Parts Discussed in Thread: DS125BR111 Hello,
My customer wants to use the SN75LVCP600S for a 2.5Gbps application, I have the IBIS model for the SN75LVCP601S part, I have seen responses in the E2E forum that the 2 parts are…
Part Number: SN75LVCP601
Do the control pins on the SN74LVCP601 have internal pull-up and/or pull-down resistors, specifically DEW1, DEW2, DE1, DE2, EQ1, and EQ2?
Part Number: SN75LVCP601 Other Parts Discussed in Thread: TUSB522P Hi Team,
Is there any objection or pitfalls in using the SN75LVCP601 as an alternative to the TUSB522P to redrive USB3.0 signals? Reason I ask is that customer is already using the SN75LVCP601…
Part Number: SN75LVCP601 Other Parts Discussed in Thread: SN75LVCP600 Hello Team;
Could you inform what is minimum storage temperature for SN75LVCP601?
Does it same as SN75LVCP600 which is -65deg.(Max =150deg.)?
Macs
Part Number: SN75LVCP601 we want use SN75LVCP601 for our new design, I have question regarding the ac-coupling capacitors on SATA high speed signals, do we actually need them? we don't need hot-plug capable.
Part Number: SN75LVCP601 Other Parts Discussed in Thread: DS64BR111 Dear Team,
I need guidance for a redesign.
Requirements for an application changed and the ambient temperature profile shows a minimum Ta = -40degC
Question:
- Can SN75LVCP601RTJR be used…