Part Number: SN75LVPE4410 Other Parts Discussed in Thread: DS160PR410 , The DS160PR410 does support EEPROM program. Does SN75LVPE4410 support EEPEOM programing?
Part Number: SN75LVPE4410
what is the function of "drv_eq_en_override" Enable overrides for driver and equalizer enables ?
Did i enable it or disable it ?
reg_06 Register
Part Number: SN75LVPE4410 It's a relate question to SN75LVPE4410: what is the function of reg_06 Register drv_eq_en_override ? - Interface forum - Interface - TI E2E support forums
We are using SN75LVPE4410 under a non PCI-e condition. And set the…
Part Number: SN75LVPE4410 We want to add a redriver for the PCIe signals going between two card modules via a backplane. In the top half of the attached PDF block diagram, we were able to connect the PCIe channels between the cards without redrivers and…
Part Number: SN75LVPE4410 Other Parts Discussed in Thread: DS160PR1601 , DS320PR1601 , DS160PR810 Hi
Is there any X16 redriver IC with higher specifications than SN75LVPE4410?
Part Number: SN75LVPE4410 Other Parts Discussed in Thread: DS160PR410 , I'm not available to find the SN75LVPE4410 datasheet (nor the DS160PR410 datasheet)
Where can I find it?
Part Number: SN75LVPE4410 Hello Guys,
Good day.
Our customer wants some clarification on SN75LVPE4410 Typical Connection Schematic. On figure10 of the device datasheet, It shows 3.3V and 3.3V filtered. Is this a typo, are they similar signals?
Thanks…
Part Number: SN75LVPE4410
Our customers have two questions as follows:
Please help check the SN75LVPE4410 schematic as below and any need to adjust
(1) Does SN75LVPE4410 Re-driver have the ability to enhance the Tx signal? If so, which Register should…