Morikeh Daramy said: "C:/ti/ motorware /motorware_1_01_00_16/sw/solutions/instaspin_foc/src/proj_lab04.c", line 110: error #148: declaration is incompatible with "Uint16 RamfuncsLoadStart" (declared at line 88 of "C:\tidcs\c28\DSP2802x\v126\DSP2802x_common…
Hi,
Why don't you download controlSuite? It has all the examples you require with documentation.
Else you can directly download F28027's Peripheral examples and headers files: http://www.ti.com/tool/sprc832
Regards,
Gautam
I believe that folder come from the 2802x peripheral examples:
http://www.ti.com/tool/sprc832
Dennis G��tz said: The next step after finding the folder, is how can i change the folder in matlab?
I don't know simulink very well but I think once you install…
Hi,
Try, 2802x C/C++ Header Files and Peripheral Examples ( http://www.ti.com/tool/sprc832 )
The above link contains a number of simple example projects for each
peripheral in F2802x device. This should be a great way to start which
allows the user…
Also, try, 2802x C/C++ Header Files and Peripheral Examples ( http://www.ti.com/tool/sprc832 )
The above link contains a number of simple example projects for each peripheral in F28027 device. This should be a great way to start which allows the user to…
All three of the low power mode code examples are included in the software package.
For CCSv4 find this in the www.ti.com/controlsuite install
Desktop GUI: Devices: View All 35+ Projects
or directly at
C:\ti\controlSUITE\device_support\f2802x\v127…
I don't know if there is an issue with the .cmd file included with CCS4, but I suggest starting out with some of the examples in the 2802x C/C++ Header Files and Peripheral Examples (SPRC832).
If you still have issues, then please post what the linker…