Part Number: SPRC892 Tool/software: Code Composer Studio I am using the following code to measure the low speed (it is basically the example "eqep_pos_speed" with minor modifications as indicated below)
// ********** LOW SPEED MEASUREMENT*…
The exmple code for the eqep_pos_speed example has the following code:
//**** Low-speed computation using QEP capture counter ****// if(EQep1Regs.QEPSTS.bit.UPEVNT==1) // Unit position event { if(EQep1Regs.QEPSTS.bit.COEF==0) …
Part Number: TMDSDOCK28035 Other Parts Discussed in Thread: SPRC191 , C2000WARE Tool/software: Code Composer Studio How do I get a down load of DSP2803x C/C++ Header and Example Files for Linux? sprc892 and sprc191 are only for installing for windows.
Also, a MathWorks rep advised me to download SPRC892 which is necessary for the for the IDE link between CCS and ML. It says that it is for XP, 2000, etc. but not Win 7. Do you know if there is an equivalent for Win 7? I haven't had an opportunity to…
Another strange thing - now it's working :)
Like there was no reason not to work, there was no reason to start working as well. I just reinstalled sprc892 and now everything is OK... I still wonder, how could the watchdog interrupt fire, but now…
EDIT - THIS CODE IS NOW INCLUDED IN THE 2803x HEADER FILES AND PERIPHERAL EXAMPLES (SPRC892)
C2000 Gurus,
I've attached a CLA example that implements an FIR filter. This code loads into flash and is copied to CLA program RAM for runtime. It requires…
There is a CLA/ADC example in the most recent version of the 2803x header files. Take a look at this and see if it resolves your question.
http://focus.ti.com/docs/toolsw/folders/print/sprc892.html
Best,
Matthew
Download, install, and read the quickstart guide. Then look at the examples directory and see the SPI folders.
http://focus.ti.com/docs/toolsw/folders/print/sprc892.html
Thanks very much. Now I'm starting to like CCSv4.
I’m trying to open the CCSV4 samples projects from F2803X Header and examples files version 1.10 (SPRC892), but I don’t know how to do it.