Hi,
below is the Mathworks respond, may be helpful:
#############################################
Try installing the following support files from TI: http://focus.ti.com/docs/toolsw/folders/print/sprc892.html When generating code for your model,…
Yulya,
The DRV8312-C2-Kit allows you to monitor the hall sensors and current. If you would like to change the direction and motion profile you can edit the GUI source code that is attached in the Files section of my Profile. The defines for the motor and…
MatthewPate said:
I beleive this has been updated in the most recent version of the C header files that we release. This structure is in the ADC.h and looks like this:
struct COMPHYSTCTL_BITS{ // bits description Uint16 rsvd1:1; // 0 reserved Ui…
Saravana,
I apologize for the delay.
Do you still receive this error message from CCS when using one of the TI code examples?
The TMS320F28035 code examples can be found here: http://focus.ti.com/docs/toolsw/folders/print/sprc892.html
If you have controlSuite…
The switch to internal osc is just for the flash plug-in programmer. The programming has to be done at a known frequency and the easiest way to do this on these devices is to just switch to the internal osc.
After programming you can change the clock…
If I remember well, I did a mistake in function for cla code copy.
You must copy your CLA code to RAM at runtime using a function like these in your code:
// Copy time critical code and Flash setup code to RAM // This includes the following ISR functions…
I am having trouble getting two Piccolo code examples to run right out of the box (do not get ADC to trigger CLA task, do not get interrupt on 280x side).
I am running the two examples cla_adc cla_adc_fir contained in the DSP2803x_examples directory which…
BJornsn,
1. Are there schematics to use in EAGLE that show me an example of
how to connect the pins of the uC with peripherals (current sensing and
ADC voltage levelling) and how to set up "housekeeping" circuitry (i.e.
voltage supply)?
-Each…