Part Number: SRC4184 Hello,Team,
I have questions about SRC4184IPAGT and CDCE913PW
・SRC4184IPAGT Q1 Are there any AC Operating Conditions which is related with RCKI, for example, setup,hold and synchronization with BCKI/O,LRCKI/O,TDMIand so on. Q2 According…
Part Number: SRC4184 Other Parts Discussed in Thread: SRC4194 Hello Professional, I have questions for SRC4184. First, Can this device continue to output I2S LRCK and BCLK signal when I2S input is lost. Second, Is SRC4184 pin and software(under HW mode)…
Part Number: SRC4184 Hi,
We have one customer who is asking if it's okay to float either one of below two pins:
SDINA - SRC A Audio Input Data
SDINB - SRC B Audio Input Data
We know that the two Sources can function independently but we do not know…
Part Number: SRC4184 Hi,
For SRC4184,both input and output ports are slave mode,
we find even when there is no input on SDIN(low level)or disconnect, SDOUT still output signal which can be seen on Oscilloscope.
Is it normal?Does the signal make sense…
Part Number: SRC4184 In slave mode, the SRC4184 is configured as an input pin and operates at rates from 32fs to 128fs.
What would happen if we provide a bit clock that is 256fs?
Are there alternative parts that would be more appropriate for the 256fs…
Part Number: SRC4184
I have a customer using the device in slave mode on all four interfaces.
Customer has a question regarding /RST pin toggling upon startup to assert device reset sequence. Is the 500ns min delay between toggling /RST low->high necessary…
Part Number: SRC4184 Hi,
Our customer has questions about SRC4184. I'm posting the question for the customer:
1)
In BYPASS mode, the BCKI/LRCKI signals are NOT directly routed to the BCKO/LRCKO. They are handled internally like NORMAL operation.
Is…
Part Number: SRC4184 Other Parts Discussed in Thread: TPS3836
One concern I have regrading the SRC4184 is how to implement the reset. The data sheet indicates that the reset must be done external to the device since it does not have an internal power…