Part Number: SRC4190-Q1 Tool/software: Hi team,
Could you please address the SRC4190-Q1 question below?
In case the system #1 and #2 are independently working:
IN_CK1 and IN_CK2's frequency and phase are both synchronized. However, the phase has a slight…
Part Number: SRC4190 Tool/software: SRC4190 is supposed to operate with a +3.3V single power supply (VDD). Are there any regulations that should be followed for the order and timing of power on and off for the I/O power supply (VIO) and VDD? For example…
Part Number: SRC4190 Tool/software: Hello team,
Could you give us the best alternative for SRC4190IDBR? (logevisty, price,,,) My customer wants to use in 15 years.
Thank you,
Alisa
Part Number: SRC4190-Q1 Can the device be used with word lengths less than 16 bit (down to 8)? Ik want to use the device in I2S mode with a number of different word lengths and sample rates.
Part Number: SRC4190-Q1 Hello expert,
Could you please measure quiescent current under following condition?
VDD:3.6V
Fsin=Fsout=48kHz
Ta=85℃
Unfortunately, there isn't EVM of this device so we cannot measure this parameter by myself...
Thank you…
Part Number: SRC4190 Other Parts Discussed in Thread: SRC4192EVM , , SRC4192 Hello Experts, My customer has question as follows. Would you answer it, please? 1. Regarding EVM, customer would like to evaluate SRC4190 by using SRC4192EVM. Can it be used? If…
Part Number: SRC4190 Hello Experts, My customer would like to use RCKI=49MHz in input/output are slave mode. Is there any concern? The sampling rate will be 192KHz. Best Regards, Fujiwara
Part Number: SRC4190 Other Parts Discussed in Thread: SRC4192 Hi, experts
My customer have some question about SRC.
Can you please confirm the following for RST on 13PIN? - What is the state of each port when RST is low?
- How long does it take the recovery…
Part Number: SRC4190 Hello team,
My customer wants to know specification of this device.
Do you have any data of power dissipation at fsout = 48kHz ?
Thanks,
Shoo
Part Number: SRC4190 Other Parts Discussed in Thread: SRC4184 , I'm designing a new circuit board and I need to transfer an audio source from IC A to IC B on the board. Both IC A and IC B have an I2S 8ch (4 data lines) master mode interface, so a sample…