Part Number: SRC4190
Hi,
On page 23 of the data sheet "Table 3. Output Port Data Format Selection", OWL1/OWL2 is mentioned. Is OWL1 -> OWL1 and OWL2 -> OWL0 correct?
Best Regards,
Nishie
Part Number: SRC4190-Q1 Hello expert,
Could you please measure quiescent current under following condition?
VDD:3.6V
Fsin=Fsout=48kHz
Ta=85℃
Unfortunately, there isn't EVM of this device so we cannot measure this parameter by myself... …
Part Number: SRC4190-Q1 Hello Expert, My customer is using SRC4190-Q1. Also they are considering to optimize their system's cost now.
Then, they are confirming the possibility of removing 10uF decupling capacitor with SRC4190-Q1 even though our recommendation…
Part Number: SRC4190 Other Parts Discussed in Thread: TLV320AIC3204 , Hello the community,
i have two I2S host configured as a master (both generates LRCLK and BCLK), i want to send the audio data output of one host to the data input of the other…
Part Number: SRC4190-Q1 Other Parts Discussed in Thread: SRC4190 Dear team,
Could you please help share with me the thermal information for our device? What is the value of θJA,θJB、θJC?
My customer is looking for asynchronous_sample_rate_converter…
Part Number: SRC4190-Q1 Hello, Team,
We have 3 questions about input and output of SRC4190-Q1.
When input audio format is set to 24 bit I2S and actual inputted data is 16bit I2S, would there be a problem?
With the above setting, can we set output…
Part Number: SRC4190 Hi Sirs, Would you please assist us to review the below block diagram if it can support customer's input clock schemes properly? 1. I2S BCLK = 1.536MHz, I2S LRCLK = 48KHz 2A. I2S BCLK = 1.4112MHz, I2S LRCLK = 441.KHz 2B. I2S BCLK…
Part Number: SRC4190
Hi,
Please confirm if SRC4190 can support a fixed 48K output and how ? the input data rate need to support from 44.1K to 192K. thanks.
Part Number: SRC4190 Hi,
I have some questions about SRC4190 when it is in Slave-Slave (input and output both slave) mode:
It needs a reference clock (pin RCKI) even if it operates in Slave-Slave mode, right?
What is the requirement of RCKI? …