Part Number: SRC4190-Q1 Other Parts Discussed in Thread: CC2560 , TLV320ADC3101 , SRC4190 Hello, Team,
My customer is inputting signal from TLV320ADC3101 to CC2560 with "DSP mode" stated in the datasheet of TLV320ADC3101.
Is it possible to input from…
Part Number: SRC4190-Q1 Is there junction temperature rating information available for this part?
The datasheet seems to show only the operating ambient temperature rating.
Is there any similar SRC part available or in development that’s rated for…
Part Number: SRC4190 Ho Sirs, For those BT system with no MCLK, can we use a discrete oscillator as SRC4190's MCLK source as the block below? Thank you and Best regards, Wayne Chen 06/25/2018
Part Number: SRC4190-Q1
Hello, Team,
SRC4190-Q1 is capable of accepting TDM input with TDMI input while also inputting I2S via SDIN. Based on this, our customer is thinking to use SRC4190-Q1 with a setting below:
If data is inputted to TDMI, would…
Hi Oinaga-san,
The purpose of Figure 2 in the SRC4190 datasheet is to visually describe the maximum clock speed and the duty cycle limits of the clock which is 50MHz and 60/40 duty cycle. Ideally you would have 50/50 duty cycle. Does that help to clarify…
Part Number: SRC4190-Q1 Hi TI-team
I understand that the RESET period needs more than 500ns.
1. How does the IC behave if the RST(RSTB) is changed from L to H with a time of 500ns or less ?
2.Are there any restrictions on the RST(RSTB) signal rise…
Part Number: SRC4190
Hi,
We are looking for suitable SRC chip which can handle a wide range of input sampling rate and the output sampling rate will be fixed at 48kHz or 96kHz. It seems that SRC4190 is a right choice, I would like to confirm that…
Part Number: SRC4190-Q1 Hello Team,
I have some question about clock.
Q. If the both port operate in Slave mode, We don't need input RCKI. Is it correct?
Q. In the Table 1, (MODE2,MODE1,MODE0)=(0,0,0) and (1,0,0) is completely same setting?
Q…
Part Number: SRC4190-Q1 HI
The current consumption at fs = 192KHz is Typ66mA in the data sheet.
What is the current consumption when fs = 48KHz?
How much does the current consumption decrease when fs = 48KHz compared to fs = 192KHz?
best …
Part Number: SRC4190-Q1 Other Parts Discussed in Thread: PCM1754-Q1 Hello Team,
Customer want to use SRC4190-Q1 and PCM1754-Q1
Q. Is there any problem if they use the combination of SRC4190-Q1 and PCM1754-Q1?
Q. Is there example block diagram or…