Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Part Number: SRC4190 Ho Sirs, For those BT system with no MCLK, can we use a discrete oscillator as SRC4190's MCLK source as the block below? Thank you and Best regards, Wayne Chen 06/25/2018
Part Number: SRC4190 Other Parts Discussed in Thread: SRC4192 , Hi Team,
Could you please advise if we have any device similar to the AK4127?
Thanks!
Roy Hsu
Part Number: SRC4190
Hi,
We are looking for suitable SRC chip which can handle a wide range of input sampling rate and the output sampling rate will be fixed at 48kHz or 96kHz. It seems that SRC4190 is a right choice, I would like to confirm that it…
Part Number: SRC4190 Hi,
The SRC4190 datasheet mentions there is a power down mode. See: * first page under 'Features' -> Power down mode * in the electrical characteristics the power usage under power down is even specified (660µW).
However…
Part Number: SRC4190
Hi Sirs, We have two SRC4190's questions need to consult with product line: 1. Customer's Codec has no MCLK output. Can we use a discrete 12.288MHz or 24.576MHz oscillator to send RCKI signal to the SRC4190? 2. If we program the…
Part Number: SRC4190 Other Parts Discussed in Thread: SRC4192 , PCM5142
I'm question about the behavior of SRC4190 Bypass pin.
When I set to Normal Mode (BYPAS = 0), the output sampling freq is 96kHz which it what I expected.
Below is the measurement…
Part Number: SRC4190 Hi all,
In a design I'm working on I need to connect two devices over I2S. Obviously one has data input and the other data output, but, unlike many other devices (especially the receiver), both devices want to be the I2S clock master…
Part Number: SRC4190 Hi Sirs,
Sorry to bother you.
As title, we would like search solution do ADSC between ADI ADV7619 and FPGA
Does SRC4190 is suitable solution?
If not, have others solution can do it?
Thanks!!
Other Parts Discussed in Thread: SRC4192 , SRC4190 , SRC4382 Hi Ti members
Purpose : "I2S to SPDIF" Solution
Test equipment -> Audio Precision AP2700 (AP)
Test condition :
AP generate 1K sine wave 0dB to EUT ---> EUT throught the " I2S to SPIF…