Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Part Number: SRC4382 Other Parts Discussed in Thread: DIX4192 , SRC4392 , , SRC4190 Hello,
Do we have a p2p alternative to the CS8422 from Cirrus Logic? It is EOL.
Best regards,
Ambroise
Other Parts Discussed in Thread: SRC4190 Hi,
I am searching a SRC to convert I2S audio sample rate in our design.
SRC4190 seems meet our requirement:
There is a HDMI Rx in our board and it capture HDMI audio as I2S signal(sample rate range: 32KHz ~ 192KHz…
Hello Diego,
I stumbled on this after having the same problem and just posted on e2e.ti.com/.../541941
My issue here is that the data sheet does NOT specify that BCKI must be 64Fs. Page 16 states "The
audio data word length may be up to 24 bits…
Hi,
6 weeks gone by without a reply to my simple question.
Does the SRC4190 support a slave input in I2S mode of 32Fs with one clock per bit at 44.1KHz as described above assuming an MCLK of 12.288MHz?
Other Parts Discussed in Thread: SRC4190 We plan to use the SRC4190 in "24-Bit LEFT Justified" input format and "24-bit/Left Justified" output format. Both input and output are in Slave-mode.
For the input format, the datasheet says…
Hi
I am also working on a design with SRC4190 . Please I would like to know the chip you used for the RESET. I am using MCP130. I have attached here my schematic, Please check if it is correct. I have some doubts
Kind regards
SOSO
Other Parts Discussed in Thread: SRC4190 Dear Justin,
I have made a schematic for SRC4190 which I want to use with the CS8416 to keep the sampling frequency at constant 192KHZ. I have attached here the schematic. I am using the clock form the I2S bus of…
Other Parts Discussed in Thread: SRC4190 Hi All,
We have used SRC4190 in our design with both input and output ports in slave mode and both are in I2S modes.
Reference clock is 24.576MHz continuous clock and output port's clock is present always. We have…
Hello Pavel,
Thanks for the feedback. I have made some changes in the schematic. I am using your schematic for the CS8164 S/PDIF decoder. I have changed the SPDIF input to AES/EBU input. I have also removed the ground on the Transformer and pin RXN…
Other Parts Discussed in Thread: SRC4190 Hi,
We are using SRC4190 with input and output sampling frequency of 48kHz as an asynchronous sample rate converter. In the datasheet, the THD is not mentioned for these input and output frequencies.
Please let…